STM32CubeMX (MCUs)

Ask questions on STM32CubeMX. Discuss code generation and configuration challenges, among other topics.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

STM32CubeMX 6.17.0 released

We are pleased to announce that version 6.17.0 of STM32CubeMX is available. What is new in 6.17.0: Added support for new microcontrollers across the STM32WBA, STM32H5, and STM32U3 seriesAdded support for new boards: NUCLEO-WBA25CE1, NUCLEO-H5E5ZJ, ST...

Aimen1 by ST Employee
  • 1756 Views
  • 0 replies
  • 2 kudos

Resolved! Trigger ADC with TIM3 on STM32L452

The reference manual states that the STM32L452 should be able to use an TIM3_TRGO as a trigger for ADC conversion:Though when I try to setup the "External Trigger Conversion Source" in STM32CubeMX there is no drop-down option for Timer 3, only TIM1/T...

0693W00000SvAYOQA3.png 0693W00000SvAZ2QAN.png
JWolf.5 by Associate
  • 1579 Views
  • 1 replies
  • 0 kudos

Resolved! Newcomer questions~Why the "SystemCoreClock" is 16000000Hz ?

I used Cubemx to configured the system clock to 180MHz. Why is the system clock in the generated project code...... 6 zeros...... 16MHz:grinning_face_with_sweat:? Can I change 16MHz to 180MHz?It simply changes the number after "SystemCoreClock" to 18...

0693W00000SvLKIQA3.png
ZeroOne by Associate III
  • 1403 Views
  • 1 replies
  • 1 kudos

FW v1.16.1 broke HAL MMC Driver

Using a custom board with an STM32F769 I had successfully interfaced to an eMMC with the HAL-MMC driver. The limitations of the driver's ability to query the extended CSD were clearly noted on this forum. I implemented my own routines to retrieve thi...

NBrow.1 by Associate
  • 3234 Views
  • 4 replies
  • 1 kudos

How to fix the update issue of STM32CubeMX?

I had installed STM32cube in my desktop with windows 10.But when do the update manager, it does not work and shows that server connection is error.But I saw the update information was refreshed 17767 days and it is very strange.Thanks a lot.Saumine

CChen.14 by Associate II
  • 11816 Views
  • 8 replies
  • 0 kudos
Announcement

We’re moving the ST Community to a new platform to give you a better and more reliable community experience.