STM32CubeMX (MCUs)

Ask questions on STM32CubeMX. Discuss code generation and configuration challenges, among other topics.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

STM32CubeMX 6.17.0 released

We are pleased to announce that version 6.17.0 of STM32CubeMX is available. What is new in 6.17.0: Added support for new microcontrollers across the STM32WBA, STM32H5, and STM32U3 seriesAdded support for new boards: NUCLEO-WBA25CE1, NUCLEO-H5E5ZJ, ST...

Aimen1 by ST Employee
  • 1756 Views
  • 0 replies
  • 2 kudos

Resolved! Debugging the microcontroller

I'm just starting to learn microcontrollers, so I have a question.I have STM32F103C8T6 and STLINK V2 programmer.Connected lines SWDIO, SWCLK, SWO(PB3) and RESET In CUBE MX I choose "No Debug" or "Serial Wire" or "Trace Asynchrone SW" and in CUBE IDE ...

0693W00000bhUkrQAE.jpg 0693W00000bhUjAQAU.jpg 0693W00000bhUj0QAE.jpg 0693W00000bhUhdQAE.jpg
DMukh.2 by Associate II
  • 2974 Views
  • 1 replies
  • 0 kudos

Resolved! STM32F107RCT7, FS USB Problem

I am having trouble with USB-FS communication with STM32F107RCT7.When the board is connected to the PC via microUSB, the PC does not even detect something is connected to the PC.I know that the PC detects a new device via a pull-up resistor on either...

0693W00000bhQ6TQAU.png 0693W00000bhQ5GQAU.png 0693W00000bhQ5BQAU.png 0693W00000bhQ56QAE.png
KOkte.1 by Associate
  • 1937 Views
  • 3 replies
  • 0 kudos

Resolved! RCC Tim Prescaler selection for APB1 not working in LL

Greetings! :)Usecase:Nucleo-F756ZGCubeMx 6.8.0Set PLL to 216 Mhz,Enable RCC->Tim prescaler selection.On "Clock Configuration" set 216 Mhz for APB1 Timer clocksWhen use HAL, It works fine. PeriphCommonClock_Config() has been genereated, but if i chang...

Resolved! Update to CubeMX 6.8 adds non-working VOSRDY flag check to SystemClock_Config() on STM32F7 using LL drivers

Hi, I have a STM32F767 project I recently updated to new software release: CubeIDE 1.12, CubeMX6.8 (both from previous versions 1.11.x and 6.7). CubeMX code generator now adds a check for flag VOSRDY after setting regulator voltage scaling in SystemC...

t.decker by Senior II
  • 4900 Views
  • 7 replies
  • 3 kudos

Bug: Pins with similar labels get same label in code

I named one pin aLoadcell- and another aLoadcell+ in STM32CubeMx (v6.6.1). They both got the same C #define in the code, as both the '-' and the '+' were replaced by a '_'.​#define aLoadCell__Pin GPIO_PIN_2 #define aLoadCell__GPIO_Port GPIOC #define ...

DLoec.1 by Associate
  • 1400 Views
  • 2 replies
  • 1 kudos
Announcement

We’re moving the ST Community to a new platform to give you a better and more reliable community experience.