2023-05-11 11:00 AM
Apologies for what might be a simple question but this is my first time working with an STM32 MCU. I am working on a project to make an RPN calculator from someone who never fully completed the project documentation. I am trying to currently flash firmware to an STM32L476 and the only files given to me under the "firmware" section of the documentation are an .ioc file, some C files, and header files. I have tried using Cube IDE and Cube Programmer but even with looking at documentation and searching via google, I have no idea how I'm supposed to turn those files into something that I can actually put onto the processor. If someone could help guide me on what I have to do it would be greatly appreciated.
2023-05-11 11:54 AM
Typically you'd Build the Project (Compile and Link)
Once that's done successfully you download the firmware image (ELF, BIN or HEX file) with an ST-LINK
2023-05-11 12:26 PM
https://www.google.com/search?q=building%20a%20project%20with%20cubeide%20site%3Ayoutube.com
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.