STM32CubeMX (MCUs)

Ask questions on STM32CubeMX. Discuss code generation and configuration challenges, among other topics.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

STM32CubeMX 6.17.0 released

We are pleased to announce that version 6.17.0 of STM32CubeMX is available. What is new in 6.17.0: Added support for new microcontrollers across the STM32WBA, STM32H5, and STM32U3 seriesAdded support for new boards: NUCLEO-WBA25CE1, NUCLEO-H5E5ZJ, ST...

Aimen1 by ST Employee
  • 1756 Views
  • 0 replies
  • 2 kudos

No interrupt in SDcard with DMA on STM32L476 and CubeMX

Hi, I have an unsolved issue with SDcard.The project is based on STM32L476, the IDE is Atollic and configuration is made by STM32CucbeMX (as I do with all my designs).Without DMA (no DMA template in FATFS and no configured DMA channels) the SDcard wo...

0693W00000D0ny7QAB.png 0693W00000D0ntHQAR.png
MarcoM by Associate II
  • 4971 Views
  • 9 replies
  • 0 kudos

HAL_HCD_Disconnect_Callback called usb host stm32f429disco 1

Hi community.. I am working with stm32f429disco1 (the one with display) I created the code with cube mx and you can find it here in the attachments.. The usb host function it is not working.. I am able to get just at the beginning one connection phos...

SGasp.1 by Senior
  • 3603 Views
  • 8 replies
  • 0 kudos

Resolved! How to detect overflow when using PWM input in combined mode

I try to measure frequency and duty of a PWM input signal with an STM32G474. For this i have selected the combined channels option "PWM input on CH2" for Timer 15 in CubeMX. The measurement works well, as long as the input signal is not to slow. When...

MSchr.1 by Associate II
  • 2920 Views
  • 1 replies
  • 0 kudos

HAL_I2C_Mem_Read returns nothing?

I use MAX9611 to measure current. It has 2 register to read current. 12 bits divides 2 bytes. MSB(8 bits) and LSB(4 bits). I tried to read only MSB but I couldn't, Can anyone help me? Note: there is no externall pull up res, I configure an internal p...

_legacyfs_online_stmicro_images_0693W00000dJpJhQAK.png
MÇETİ.1 by Associate III
  • 2502 Views
  • 2 replies
  • 0 kudos

Resolved! How to change Init functions to global?

I am currently attempting to build code in simulink for a GIGA R1 project I have. However when setting the ioc file up in CubeMX I am unable to change the init functions to be global. Any help would be appreciated. Thanks!

Announcement

We’re moving the ST Community to a new platform to give you a better and more reliable community experience.