2023-06-04 1:40 AM
In STM32CubeMX 6.8.1. (and before), there is an option to enter a custom path to the firmware. But, in contrast to what it says, I can only pick an absolute path here. This is unwanted when projects are shared between users/machines. For example, I would like to store the firmware in the same git repository as a number of projects using it. Workaround: patching the generated Makefiles :(
KnarfB
2023-06-04 8:22 AM
This is a well known limitation, usually people find some workaround that works for them.
For example you can choose a single fixed location outside of any user profile (such as /opt/st/...)
You can also create symlinks to the Cube firmware location in your projects, and/or use environment variables.
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.