STM32CubeMX (MCUs)

Ask questions on STM32CubeMX. Discuss code generation and configuration challenges, among other topics.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

STM32CubeMX 6.17.0 released

We are pleased to announce that version 6.17.0 of STM32CubeMX is available. What is new in 6.17.0: Added support for new microcontrollers across the STM32WBA, STM32H5, and STM32U3 seriesAdded support for new boards: NUCLEO-WBA25CE1, NUCLEO-H5E5ZJ, ST...

Aimen1 by ST Employee
  • 1756 Views
  • 0 replies
  • 2 kudos

Resolved! Generating c++ projects with STM32CubeMX

Hi, I'm trying to make a c++ project for STM32CubeIDE using the STM32CubeMX.However there doesn't seem to be any c++ option, is there something I'm missing or is the software just not made for it?

Resolved! Where to find BOOT1 on STM32F415?

The manual for the STM32F415 says that the BOOT1 signal "...is shared with a GPIO pin", but it doesn't say actually which pin. CubeMX does not show it either. I've seen online that at least for some other MCU's in the F4 range, BOOT1 is mapped on PB2...

RHarte by Associate II
  • 2343 Views
  • 2 replies
  • 0 kudos

Why is there a pulse on ADC input channel

I use ADC0 and ADC1 of STM32F334,I put a resistor of 1K between amplifier and ADC channel, configuring every IO setting by using CubeMX, but I find something strange, there is a pulse on ADC input pin,while amplier output is flat. And the result read...

_legacyfs_online_stmicro_images_0693W00000bkoP6QAI.png
WSuke.1 by Associate
  • 1340 Views
  • 1 replies
  • 0 kudos

Resolved! HardFault after EXTI and starting & resetting timer SOLVED

HiI get a hardfault as soon as the HALL sensor (which is connected & set up using CubeMX & EXTI GPI(O)) gets an interrupt.I have debugged the code to the part where I can safely say that the hard fault only occurs when the " __HAL_TIM_SET_COUNTER(&ht...

Lixx by Associate III
  • 4575 Views
  • 7 replies
  • 0 kudos
Announcement

We’re moving the ST Community to a new platform to give you a better and more reliable community experience.