STM32CubeMX (MCUs)

Ask questions on STM32CubeMX. Discuss code generation and configuration challenges, among other topics.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

STM32CubeMX 6.17.0 released

We are pleased to announce that version 6.17.0 of STM32CubeMX is available. What is new in 6.17.0: Added support for new microcontrollers across the STM32WBA, STM32H5, and STM32U3 seriesAdded support for new boards: NUCLEO-WBA25CE1, NUCLEO-H5E5ZJ, ST...

Aimen1 by ST Employee
  • 1756 Views
  • 0 replies
  • 2 kudos

Resolved! WolfSSL code not being generated completed from CubeMX

Hey all, I am attempting to use the CubeMX to enable and generate code for the WolfSSL middleware.   When I do, it seems to not generate all the files.  One that is missing for example is evp.c.  However, it seems that none of the .C files are genera...

vanhorng_0-1694533986762.png vanhorng_1-1694534568127.png
vanhorng by Associate
  • 2426 Views
  • 2 replies
  • 0 kudos

CubeMX 6.9.1 doesn't see CubeF7 1.17.1

Saw issue in another thread about CubeIDE 1.13.1 unable to generate code from F7 1.17.1 (https://community.st.com/t5/stm32cubeide-mcus/stm32cubeide-v1-31-1-error-when-using-1-17-1-fw-patch/td-p/588887).Interestingly, CubeMX v6.9.1 (Windows) won't eve...

Bob S by Super User
  • 4189 Views
  • 5 replies
  • 0 kudos

ADC conversion mixing channels values

I'm working on a project in speed control of a pmsm and i am using ADC1 and 7 channels of the ADC to sample 7 different inputs. The ADC gets triggered from TIM2 and i'm doing the conversions every time i get a callback. At first the adc works fine wi...

Resolved! Make can not build project from STM32CubeMX with CMSIS_V2

I encountered a problem with building project from STM32CubeMX v6.9.1 with generated Makefile and CMSIS_V2 enabled. Starting build by 'make' returns an error 1 for /main.o "Can not find specified file". On the other hand, when using CMSIS_V1 everythi...

Michał M by Associate II
  • 1665 Views
  • 1 replies
  • 0 kudos

Resolved! Make can not build project from STM32CubeMX with CMSIS_V2

I encountered a problem with building project from STM32CubeMX v6.9.1 with generated Makefile and CMSIS_V2 enabled. Starting build by 'make' returns an error 1 for /main.o "Can not find specified file". On the other hand, when using CMSIS_V1 everythi...

Michał M by Associate II
  • 1941 Views
  • 2 replies
  • 0 kudos

STM32CubeMX 6.9.1 and STM32CubeIDE 1.13.1 released.

STM32CubeIDE 1.13.1 was released on st.com as well as an in-tool update patch aligned with STM32CubeMX v6.9.1 that is available for download.Main issues fixed in this patch:This patch release fixes the issues related to the following cases:STM32CubeM...

Resolved! LWIP - udp_new() returns PCB as NULL

Hi,I decided to upgrade my STM32CubeMX to the latest version 6.9.1.my project was generated first with STM32CubeMX 6.5.0 - so I had to copy the IOC manually.I checked multiple times that all configuration is the same like it was, and it is. when I'm ...

Mz.1 by Associate III
  • 4422 Views
  • 3 replies
  • 1 kudos

Disable auto comment generation

I understand the reason behind it and it is a very useful feature, but please add the option to disable it when it's not needed. Most of the time I just do a one-off configuration using the cube configurator and then I write my own code. Also, the wa...

BSerb by Associate II
  • 2268 Views
  • 2 replies
  • 0 kudos
Announcement

We’re moving the ST Community to a new platform to give you a better and more reliable community experience.