STM32CubeMX (MCUs)

Ask questions on STM32CubeMX. Discuss code generation and configuration challenges, among other topics.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

STM32CubeMX 6.17.0 released

We are pleased to announce that version 6.17.0 of STM32CubeMX is available. What is new in 6.17.0: Added support for new microcontrollers across the STM32WBA, STM32H5, and STM32U3 seriesAdded support for new boards: NUCLEO-WBA25CE1, NUCLEO-H5E5ZJ, ST...

Aimen1 by ST Employee
  • 1757 Views
  • 0 replies
  • 2 kudos

CUBE AI 8.1.0 does not run

Hello, I saw the link below and ran it.// Set pointers wrapper structs to our data buffersai_input[0].n_batches = 1;ai_input[0].data = AI_HANDLE_PTR(in_data);ai_output[0].n_batches = 1;ai_output[0].data = AI_HANDLE_PTR(out_data);An error is occurring...

Missing Files when exporting project using STM32CubeMX

Dear Sir/Madam, Good day. Here I am facing the problem of missing generated files when building project using STM32 CubeMX software here I am sending image of which files are missing please provide us your kind support i am a beginner thank you best ...

image.png

Option/feature suggestion - Discussion CubeMX

I had changed a library file, and i wondered, why after a MX config generation it did not work anymore.CubeMX replaced all the files!!! Lucky i had some backup. Why would you replace library files, that were already copied? Please see my picture for ...

Tobe by Senior III
  • 4292 Views
  • 7 replies
  • 1 kudos

Resolved! Problem with CubeMX after upgrading - can't open ioc file

I upgraded STM32CubeIDE to 1.14.0 and then when I went to open an ioc file I got this message:This project was setup with STM32CubeMX V6.9.2 using STMCube FW_G0 V1.6.1.There are two options to proceed:-Migrate:Migrate your project using the current S...

Dabbo by Associate III
  • 10719 Views
  • 10 replies
  • 0 kudos

SDCARD does not work with 4bits wide bus

Hi I have STM32F407 and after updating STM32CubeMX 6.6.1 -> 6.9.2 I faced the same issue with SD card:https://community.st.com/t5/stm32cubemx-mcus/sdcard-does-not-work-fr-not-ready-when-migrating-from-fw-f4-v1/m-p/115499#M3876It seems that with previ...

JBond.1 by Senior II
  • 8682 Views
  • 8 replies
  • 2 kudos

Resolved! How Ethernet MAC interrupts have been enabled by STM32CubeH7?

Hi all. This is the first time I am using CubeH7 + FreeRTOS + LwIP. I have tried to trace down how Ethernet MAC interrupts have been enabled. If I got the code correctly:+ I enabled "Ethernet global interrupt" option from CubeMX "ETH".+ I enabled "Lw...

Leon_MS by Associate III
  • 2751 Views
  • 2 replies
  • 0 kudos
Announcement

We’re moving the ST Community to a new platform to give you a better and more reliable community experience.