2023-11-30 4:11 PM
I have Nucleo STM32U5A5 board where I experiment with the USBX interface based on demo code. I then created new project to experiment with GPDMA. Both IDE and MX are updated at the time of 30/Nov/23.
It keep on repeating RCC/PWR setup warning or issue when I run generate code. When I went back to demo code: Ux_Device_CDC_ACM, I also generated the code from CubeMX with added USART2. It produce same RCC/PWR error. It seen to point to PWR privilege and RCC privilege (with !) on it. I have not activated trustzone.
Can you advise what should I do about it, is there bug in these or workaround?
2023-11-30 5:37 PM
And what is the warning? Hover over it for more information.
Yellow warnings generally do not indicate issues and can be ignored. Red errors show actual issues.
2023-12-01 7:21 AM
2023-12-01 8:09 AM - edited 2023-12-01 8:11 AM
Doesn't look like you show the clock tree in the PDF. Presumably the error is in there.
Can you attach your IOC file. Rename it from .ioc to .txt to get around the inexplicable forum filter.
At a guess, increase the power regulator voltage scale to 1 to allow for higher clock speed.
2023-12-01 8:25 AM
2023-12-01 8:51 AM
Okay, I can replicate. I can't really explain why that's happening, but changing RCC parameter to bypass, then back to crystal gets rid of the RCC warning. And unchecking and rechecking any option in PWR gets rid of the PWR warning. It then generates code without warning.
2023-12-01 8:52 AM
It looks like the toolchain parameter is not properly set in the IOC file that you sent. Setting it to STM32CubeIDE fixes the issue.
2023-12-01 9:04 AM
Before I generated the code, I edited it with Visual Code and added as you indicated
ProjectManager.PreviousToolchain=STM32CubeIDE
I then saved the file and generated code via STM32CubeIDE, which still reports the error below.
- Main Config: These peripherals still have some not configured or wrong parameter values: [PWR, RCC]
I inspected the ioc file and it reverted back to blank.
ProjectManager.PreviousToolchain =
How to generate code without clearing it?
Thanks
2023-12-01 9:34 AM
2023-12-01 9:57 AM
Ok
I have removed the isbadioc line (via Visual code) but now it mask out the Generate Code in the context menu from ioc filename in the STM32CubeIDE. I feel it outsmarted me to make progress!.
.
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.