STM32CubeMX (MCUs)

Ask questions on STM32CubeMX. Discuss code generation and configuration challenges, among other topics.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

STM32CubeMX 6.17.0 released

We are pleased to announce that version 6.17.0 of STM32CubeMX is available. What is new in 6.17.0: Added support for new microcontrollers across the STM32WBA, STM32H5, and STM32U3 seriesAdded support for new boards: NUCLEO-WBA25CE1, NUCLEO-H5E5ZJ, ST...

Aimen1 by ST Employee
  • 1762 Views
  • 0 replies
  • 2 kudos

Re: Connecting SD CARD to STM32H743 without level translator

Guys I just don't get this part in CubeMX. What does it mean by "voltage converter"? Does it refer to voltage translator? In that case why would a software stack cares about a voltage translator (which is basically a 1:1 interface) and changes the si...

0.png
Mosi by Associate II
  • 1302 Views
  • 1 replies
  • 0 kudos

My CubeMX UI is messed up.

I do apologize if this is in wrong section or something. I just don't have time to spend hours looking for correct place to get support. I need to work, not fiddle with misbehaving software.The issue I am having is that CubeMX (latest version from th...

0690X000006CqcAQAS.jpg 0690X000006Cqc5QAC.jpg
EKokk by Associate II
  • 9071 Views
  • 15 replies
  • 2 kudos

STM32cubeMX - Change processor type

Posted on September 02, 2015 at 18:03Is it possible the change the selected processor in a given STM32cubeMX project? I would like to maintain the user pin labels and config. #stm32cubemx

Resolved! incorrect code generated for OCTOSPI on STM32H725

STM32CubeMX generates incorrect code for the OCTOSPI interface for STM32H725.The generated code does not populate the Req2AckTime field of the OSPIM_CfgTypeDef structure, but HAL_OSPIM_Config() validates this value and throws an assertion error. See ...

0693W00000QKm66QAD.jpg

Resolved! Issue in FW F7 HAL package 1.17.x

Hi,i have STM32F767BIT6 MCU and microcontroller crashes into Hard Fault during initialisation of LWIP MX_LWIP_Init(); Problem is that in FreeRTOS is calling memcpy in queue.c in function prvCopyDataFromQueue with huge ammount of length.( void ) memcp...

Petr3 by Associate III
  • 6121 Views
  • 11 replies
  • 2 kudos
Announcement

We’re moving the ST Community to a new platform to give you a better and more reliable community experience.