STM32CubeMX (MCUs)

Ask questions on STM32CubeMX. Discuss code generation and configuration challenges, among other topics.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

STM32CubeMX 6.17.0 released

We are pleased to announce that version 6.17.0 of STM32CubeMX is available. What is new in 6.17.0: Added support for new microcontrollers across the STM32WBA, STM32H5, and STM32U3 seriesAdded support for new boards: NUCLEO-WBA25CE1, NUCLEO-H5E5ZJ, ST...

Aimen1 by ST Employee
  • 1756 Views
  • 0 replies
  • 2 kudos

Dual Bank Linker script for STM32G474CB

HelloI have a project with STM32G474CB in CubeMX and it generates the linker script with following:  MEMORY { RAM (xrw) : ORIGIN = 0x20000000, LENGTH = 128K FLASH (rx) : ORIGIN = 0x8000000, LENGTH = 128K } But, as I understand, th...

SMisi by Associate II
  • 1371 Views
  • 1 replies
  • 0 kudos

CubeMX: "Code generation could not be done"

Split from: https://community.st.com/t5/stm32cubeide-mcus/changes-in-ioc-file-not-updating-the-code/td-p/661312 as the OP abandoned that thread, and it's a different problem anyhow. Hello GladsonIm here because now i have the same problem of you. I d...

Problem_generation_code.png
LSZ by Associate
  • 1502 Views
  • 2 replies
  • 1 kudos

Resolved! stm32 usb device dual

Hello. I'm using EVM board with STM32F407ZGT.I set up the USB as below to use it as a USB Device. (CDC)But only one COM port can be found in the device manager on the PC.I want to know if I can't set 2 usb device or if it's a problem with setting.Ple...

2024-05-29_134310.jpg 2024-05-29_134325.jpg 2024-05-29_134405.jpg 2024-05-29_135118.jpg
DJung.3 by Associate II
  • 3081 Views
  • 3 replies
  • 0 kudos

STM32H745 RMII and DP83822 Question

I use STM32H745 RMII and DP83822 To use CubeMx generate code for lwip, selected phy is LAN8742.Modify the code But can't make it work Any body has the experience or some advice ?Hope someone can help me.

WTieg.1 by Associate II
  • 7636 Views
  • 11 replies
  • 1 kudos

Resolved! documentation on STM32 PWM fast mode

Posted on February 08, 2017 at 12:00Hiin cubeMX for any TIM PWM IO I can enable / disable 'fast mode'.What is fast mode?In which pdf document  would I find the description of fast mode, and register address? I am trying to find my way in all the dif...

STM3CubeMX no download link

Hello,Today I have been trying to install STM3CubeMX as well as the STM3Cube IDE . But , no matter what I try, I never get a download link to proceed with the download after pressing the "download latest" button on the desired software. Nothing at al...

CubeMX and STM32H753I-EVAL2 issues

Having some issues with CubeMX not showing properly the DevKit hardware features. For example:The devkit has an ST-LINK V3 chip (per documentation and according to silk screen) yet CubeMX has the ST-LINK V2 setting available only, ST-LINK V3 is greye...

armDevCP by Associate II
  • 2350 Views
  • 4 replies
  • 0 kudos
Announcement

We’re moving the ST Community to a new platform to give you a better and more reliable community experience.