2024-11-13 11:50 PM
Hello
I have a project with STM32G474CB in CubeMX and it generates the linker script with following:
MEMORY
{
RAM (xrw) : ORIGIN = 0x20000000, LENGTH = 128K
FLASH (rx) : ORIGIN = 0x8000000, LENGTH = 128K
}
But, as I understand, this is only the case when the device is switched into single-bank mode (which is not the default from the manufacturer!). The default would be two 64K flash chunks with second being at offset 0x08040000, am I correct?
Thanks.
2024-11-14 12:25 AM - edited 2024-11-14 12:53 AM
Hello @SMisi
On this, the RM0440 clearly states they're consecutive in single bank mode.
Your question is answered nicely by ST here:
The STM32CubeMX generated script is correct for single bank mode.
THX
Ghofrane
To give better visibility on the answered topics, please click on Accept as Solution on the reply which solved your issue or answered your question.
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.