2017-02-08 3:00 AM
Hi
in cubeMX for any TIM PWM IO I can enable / disable 'fast mode'.
What is fast mode?
In which pdf document would I find the description of fast mode, and register address? I am trying to find my way in all the different documentation pdfs!
Thx
#pwm #cube-mxSolved! Go to Solution.
2017-02-08 7:36 AM
Hi
dieter.dieter
,Fast-mode (Fm)is applicable only for I2C pins.FT_f I/O pins support Fm+ mode which is configured in the SYSCFG_CFGR1 register.
Refer to the RM0351 reference manual onpage276(System configuration controller (SYSCFG) section)for more details and in '35 Inter-integrated circuit (I2C) interface' section.
Inthe STM32L476xx
, refer to these tables:Table Legend/abbreviations used in the pinout table
Table STM32L476xxSTM32L476xx pin definitions
Hope this helps you.
Regards
Imen
2017-02-08 4:57 AM
Hello
dieter.dieter
,You should review your reference manual related to your device for more clarification about TIM, PWM mode and register address.
Regards
Imen
2017-02-08 6:15 AM
Hi
DAHMEN.IMEN
could you refer me to page and chapter where it is described?I am using a STM32L4x6!
I searched for 'fast mode' and 'fast-mode' in these 2 documents:
1.STM32L476xx datasheet
2. RM0351 Reference manual
I couldn't find it!
Thx
2017-02-08 7:36 AM
Hi
dieter.dieter
,Fast-mode (Fm)is applicable only for I2C pins.FT_f I/O pins support Fm+ mode which is configured in the SYSCFG_CFGR1 register.
Refer to the RM0351 reference manual onpage276(System configuration controller (SYSCFG) section)for more details and in '35 Inter-integrated circuit (I2C) interface' section.
Inthe STM32L476xx
, refer to these tables:Table Legend/abbreviations used in the pinout table
Table STM32L476xxSTM32L476xx pin definitions
Hope this helps you.
Regards
Imen
2017-02-09 1:01 AM
I don't CubeMX, but this sounds like:
Reference Manual (I used RM0090 but I bet this is the same accross all STM32), Timer chapter:
Particular case: OCx fast enable:
In One-pulse mode, the edge detection on TIx input set the CEN bit which enables thecounter. Then the comparison between the counter and the compare value makes theoutput toggle. But several clock cycles are needed for these operations and it limits theminimum delay t DELAY min we can get.To output a waveform with the minimum delay, the user can set the OCxFE bit in theTIMx_CCMRx register. Then OCxRef (and OCx) is forced in response to the stimulus,without taking in account the comparison. Its new level is the same as if a compare matchhad occurred. OCxFE acts only if the channel is configured in PWM1 or PWM2 mode.JW
2017-02-09 1:41 AM
Hi
DAHMEN.IMEN
one last question remains: If fast mod is related to i2c, why does this setting show up in cubemx. In pinout tab I sat up TIM1 channel1 as PWM generation channel 1. In cubemx Config tab under TIM1 , under PWM settings for channel 1 I can enable/disable fast mode. According to spec fast mode is not related to PWM but I2C.
So what does this bit do in case of PWM? I want to use pwm to dimm LEDs.
2019-03-20 2:17 AM
This is interesting. Anybody answer please? I'm curious too.
2024-04-09 3:41 PM
Not to resurrect a dead thread here, but for the benefit of others who stumble on this:
The accepted solution does not address the question. The OP was asking about PWM fast mode, which is covered by JW's reference manual snippet. The accepted solution is referencing a different "fast mode" pertaining to I2C clocking speeds(ie 400Khz/1Mbit). I can see how the OP was confused by this. It doesn't help that Cube calls the setting "Fast Mode" and the reference manual refers to a "fast enable" bit. It also doesn't help that many interfaces have modes with "fast" in their name, referring either to clocking speeds, or latency as the case may be. Finally, those familiar with Arduino/AVR processor PWMs which also have a "Fast Mode" will discover that STMs fast mode appears to be a different mechanism and possibly only applying to one-pulse mode. Welcome to the Wild West of MCU exploration ;)
2024-04-10 12:55 AM - edited 2024-04-10 12:56 AM
> possibly only applying to one-pulse mode
No, they are completely mutually independent features.
> Welcome to the Wild West of MCU exploration
...as in the vast prairies of the manuals?
JW
2024-11-12 4:27 AM
I ´ve been searching for this and I found that Fast mode tab in timer setting in CubeMX mean this:
Bit 2 OC1FE: Output Compare 1 fast enable
This bit decreases the latency between a trigger event and a transition on the timer output.
It must be used in one-pulse mode (OPM bit set in TIMx_CR1 register), to have the output
pulse starting as soon as possible after the starting trigger.
0:CC1 behaves normally depending on counter and CCR1 values even when the trigger is ON. The minimum delay to activate CC1 output when an edge occurs on the trigger input
is 5 clock cycles.
1:An active edge on the trigger input acts like a compare match on CC1 output. Then, OC is set to the compare level independently of the result of the comparison. Delay to
sample the trigger input and to activate CC1 output is reduced to 3 clock cycles. OC1FE
acts only if the channel is configured in PWM1 or PWM2 mode.
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.