STM32CubeMX (MCUs)

Ask questions on STM32CubeMX. Discuss code generation and configuration challenges, among other topics.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

STM32CubeMX 6.17.0 released

We are pleased to announce that version 6.17.0 of STM32CubeMX is available. What is new in 6.17.0: Added support for new microcontrollers across the STM32WBA, STM32H5, and STM32U3 seriesAdded support for new boards: NUCLEO-WBA25CE1, NUCLEO-H5E5ZJ, ST...

Aimen1 by ST Employee
  • 1756 Views
  • 0 replies
  • 2 kudos

Resolved! STM32CubeMX 6.13.0 - SPI NSS can't select SPI_NSS_SOFT

SPI with NSSNSS Signal Type Output Software is missing in the pulldown.What did I wrong?I attached the ios file.Of course I can edit the source and never let STM32CubeMX touch the project again, but that wasn't the goal, right?   hspi1.Init.NSS = SPI...

javaw_WKW4pHUDGG.png
Jack3 by Senior III
  • 1276 Views
  • 1 replies
  • 1 kudos

Resolved! How to configure FatFs with DMA on STM32L5 using CubeMx.

Hello, I would like to have advice, I see this video about SD Card :https://www.youtube.com/watch?v=I9KDN1o6924&t=359sAnd in the video (5:30) I can see DMA tab via CubeMXBut with me I don't have this tab, do you know why ?I have STM32L552E-EV Evaluat...

DYann1_0-1736510553492.png DYann1_1-1736510815033.png
DYann.1 by Senior II
  • 3911 Views
  • 9 replies
  • 3 kudos

Resolved! DCT Issue: Missing HAL Interrupt Handler for USART6

Hi everyone,I'm encountering an issue with the STM32 Device Configuration Tool: it doesn't properly generate the global interrupt handler function for one of the UARTs in my project: The generated interrupt handlers for USART1 and USART2 include call...

How to install x-cube-eeprom on STM32Cube?

Hello, I have downloaded en.x-cube-eeprom_v4.0.0.zip but I do not know how to install it on STM32Cube. It should have been a package installed "from local" and selected the zip in STM32Cube MX? Or what I need to do is copy all the files for my projec...

FCOST.1 by Associate II
  • 13111 Views
  • 11 replies
  • 7 kudos

Installing CubeMX 6.13 -console Error

I have tried to install the latest CubeMX software 6.13 in silent mode. Unfortunately the installation fails with the following error code in debug mode: 'ProcessBuilder.start(): pid: 95163, dir: null, cmd: “net”'I have executed the installation with...

Crankzz by Associate
  • 1876 Views
  • 3 replies
  • 0 kudos

USB HS - USB_TIMEOUT in stm32h7r3z8t6

Hello,I am working on a custom board with stm32h7r3z8t6. After the definition of the USB HS in Cube MX, the USB initialization is stuck on USB_TIMEOUT: USB HS connection on the board:  Here is the clock config:  void SystemClock_Config(void){RCC_OscI...

MihavinVin_2-1736260768989.png MihavinVin_3-1736260959083.png MihavinVin_4-1736261000481.png MihavinVin_0-1736260554509.png
Announcement

We’re moving the ST Community to a new platform to give you a better and more reliable community experience.