STM32CubeMX (MCUs)

Ask questions on STM32CubeMX. Discuss code generation and configuration challenges, among other topics.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

STM32CubeMX 6.17.0 released

We are pleased to announce that version 6.17.0 of STM32CubeMX is available. What is new in 6.17.0: Added support for new microcontrollers across the STM32WBA, STM32H5, and STM32U3 seriesAdded support for new boards: NUCLEO-WBA25CE1, NUCLEO-H5E5ZJ, ST...

Aimen1 by ST Employee
  • 1756 Views
  • 0 replies
  • 2 kudos

Resolved! Automatic USART Baudrate detection for STM32H523

Hi, I have tried to configure the STM32H523RET6 for using USART1 with multiprocessor communication mode and enabled the auto baudrate detection. However, according to the application Note AN4908, the MCU stm32h523 doesn't support auto-baudrate. I don...

hakeila by Associate III
  • 1372 Views
  • 1 replies
  • 1 kudos

Resolved! OCTOSPI and MDMA - STM32CubeMX bug

Hello!I would like to report a bug. Using STM32CubeIDE 1.16.0 and the integrated STM32CubeMX 6.12.0 i encountered a bug regarding OCTOSPI and MDMA on STM32H723ZGT6 MCU. Inside HAL_SPI_Receive_DMA(handle, pdata); where the HAL_MDMA_Start_IT is called ...

samob2703_0-1722426480442.png
samob2703 by Associate II
  • 1846 Views
  • 2 replies
  • 2 kudos

Resolved! In CubeMX getting a red pin

What does a red highlight mean? I am able to select the pin for the function I want but I'm seeing at least two pins with of these red highlights. One is an GPIO output which toggles fine. The other is for an EXTI which no longer generates an interru...

JBias_1-1737426925291.png
JBias by Associate III
  • 1406 Views
  • 1 replies
  • 0 kudos

Resolved! STM32CubeMX code generation error

Hello everyone,I'm sitting over here working on one of my projects and found that STM32CubeMX generated code with an error. My project uses the STM32H7R3L8H6H MCU with Ethernet activated in the connectivity. I have my project set to "generate individ...

Intector_0-1737398906247.png

Resolved! Struggling with HSE

I am in the process of transferring from Mbed to VSCode with the STM332 extension. I have set up a project using CubeMX set to the default settings for a NUCLEO-L073 and have no issues. I believe this setup uses the MSI clock. I am trying to implemen...

pmcew by Associate II
  • 4870 Views
  • 6 replies
  • 3 kudos
Announcement

We’re moving the ST Community to a new platform to give you a better and more reliable community experience.