STM32CubeMX (MCUs)

Ask questions on STM32CubeMX. Discuss code generation and configuration challenges, among other topics.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

STM32CubeMX 6.17.0 released

We are pleased to announce that version 6.17.0 of STM32CubeMX is available. What is new in 6.17.0: Added support for new microcontrollers across the STM32WBA, STM32H5, and STM32U3 seriesAdded support for new boards: NUCLEO-WBA25CE1, NUCLEO-H5E5ZJ, ST...

Aimen1 by ST Employee
  • 1756 Views
  • 0 replies
  • 2 kudos

Resolved! Cannot assign HASH_IN as a GPDMA request source

Hello, I'm using STM32H503RBT and trying to configure a DMA transfer from memory to the HASH engine, but even though I have that peripheral configured as show on the picture below, I can't assign it as the request source for the DMA is grayed out and...

QuickSilver127_0-1738003439949.png QuickSilver127_2-1738003526527.png

STM32CubeMX bug report

Dear ST support team,In STM32CubeMX under the "Project Manager - Advanced Settings" path in the "Generated Function Calls" window user can select to make the generated functions' scope static or external. However, the SystemClock_Config() is always s...

lgacnik97 by Associate III
  • 1205 Views
  • 1 replies
  • 2 kudos

STM32CubeMX 6.13.0 released

We are pleased to announce to you that the release 6.13.0 of STM32CubeMX is available. What is new in 6.13.0: Added support for the following series, microcontrollers and microprocessors: STM32N6, STM32U3, STM32WL3x, STM32G411xx and STM32C0Added the ...

Resolved! STM32CubeMX Release 6.3.0 crached after start

I have the following big problem:I had installed previously release 6.2.0 of STM32CubeMX and everything works fine. Then i uninstall this release and update to the new one 6.3.0.Now the programm craches after start. An backgroundprocess at windows fo...

TLoew.1 by Associate
  • 2166 Views
  • 3 replies
  • 0 kudos

CubeMx: selecting Firmware Path

Why can't I change the Firmware Relative Path when I have unchecked the "Use Default Firmware Location"?I clicked the "Browse" button and there was no response.

Ryan71 by Associate II
  • 4073 Views
  • 7 replies
  • 1 kudos
Announcement

We’re moving the ST Community to a new platform to give you a better and more reliable community experience.