STM32CubeMX (MCUs)

Ask questions on STM32CubeMX. Discuss code generation and configuration challenges, among other topics.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

STM32CubeMX 6.17.0 released

We are pleased to announce that version 6.17.0 of STM32CubeMX is available. What is new in 6.17.0: Added support for new microcontrollers across the STM32WBA, STM32H5, and STM32U3 seriesAdded support for new boards: NUCLEO-WBA25CE1, NUCLEO-H5E5ZJ, ST...

Aimen1 by ST Employee
  • 1756 Views
  • 0 replies
  • 2 kudos

MxCube code generator directory structure messed up

Hi,I want to generate code and project files for MDK-ARM and STM32CubeIDE.For this I created a new directory and copied the .ioc file into it and opened it it with CubeMx (latest version 6.13).In the projectmanager/project the following directory str...

initial_view.png modified_view.png stmcubeide.png codegen_done.png
regjoe by Senior II
  • 1526 Views
  • 1 replies
  • 0 kudos

Resolved! MX_SDMMC1_SD_Init missing HAL_SD_Init

Hi, I'm using STM32CubeMX 6.13.0 and MCU STM32H753VITx.When initializing the SDMMC1, I am missing the call to function HAL_SD_Init.  void MX_SDMMC1_SD_Init(void) { /* USER CODE BEGIN SDMMC1_Init 0 */ /* USER CODE END SDMMC1_Init 0 */ /* USER...

Jack3 by Senior III
  • 1619 Views
  • 3 replies
  • 0 kudos

v6.13.0 generated comment style

I have a project I setup using STM32CubeMX v6.12.0 when I open the .ioc file in the current IDE I am prompted to migrate v6.13.0If I do this, next time I generate code the comment style of the generated code has changed from: /** * @brief The appli...

Tom_y by Associate
  • 882 Views
  • 0 replies
  • 1 kudos

CubeMX RTC config issues

Trying to to set up RTC alarm for STM32U5G9 I come across this CubeMX issues:There is no option to disable Calendar date and time setup. Needless to say, probably it does not make any sense to set up date and time on every board reset if it has (as i...

TDJ_1-1735906003846.png TDJ_2-1735907337800.png
TDJ by Lead
  • 3039 Views
  • 5 replies
  • 2 kudos

Configure RTC Alarm separately from RTC

Follow on from:https://community.st.com/t5/stm32cubemx-mcus/how-to-have-cubemx-configure-a-peripheral-but-not-enable-it/m-p/761692/highlight/true#M30801 To be able to configure the RTC Alarm in CubeMX, you have to enable it in CubeMX.This means that ...

Announcement

We’re moving the ST Community to a new platform to give you a better and more reliable community experience.