STM32CubeMX (MCUs)

Ask questions on STM32CubeMX. Discuss code generation and configuration challenges, among other topics.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

STM32CubeMX 6.17.0 released

We are pleased to announce that version 6.17.0 of STM32CubeMX is available. What is new in 6.17.0: Added support for new microcontrollers across the STM32WBA, STM32H5, and STM32U3 seriesAdded support for new boards: NUCLEO-WBA25CE1, NUCLEO-H5E5ZJ, ST...

Aimen1 by ST Employee
  • 1756 Views
  • 0 replies
  • 2 kudos

Resolved! Nucleo STM32WL33 CMake

Board: NUCLEO-WL33 Toolchain: CMake + arm-none-eabi-gcc CubeMX version: 6.17.0 STM32CubeIDE version: 2.1.1I am trying to run a basic STM32WL33 project generated by STM32CubeMX using the CMake toolchain instead of the native STM32CubeIDE project forma...

Jdescot by Associate II
  • 764 Views
  • 5 replies
  • 5 kudos

CubeMXes should assist with UCPD Dead Battery

The UCPD Dead-battery mechanism is a major gotcha in many new STM32, as it creates a surprising bond between seemingly unrelated pins, and is on by default. There cannot be enough warnings to this, as users not intending to use the PD (which is proba...

Resolved! CubeMX Route Opamp output to ADC on STM32U3C5CIUxQ

Hello,According to Table 246 in section 27.3.3 Signal Routing of the STM32U3 Reference Manual, I should be able to configure ADC1_IN6 as an ADC input when using OPAMP1, or ADC1_IN13/ADC2_IN9 when using OPAMP2 such that the output of the opamps are ro...

AQB_0-1775823813286.png AQB_1-1775823963323.png
AQB by Associate
  • 459 Views
  • 3 replies
  • 0 kudos

Resolved! DCMIPP Setup for STM32N6570-DK

I am running the pre-compiled "object Detection" files on the STM32N6570-DK and am in the process of trying to generate my own STM32CubeMX setup project for the fsbl.I am having difficulty setting up the numerous options for the DCMIPP for this proje...

digilog by Associate II
  • 1031 Views
  • 6 replies
  • 1 kudos

Resolved! CubeMX Bug Project Manager

CubeMX Project Manager has a bug, where when I accidentally cleared the "Project Location" field and moved the cursor away CubeMX complains that project location cannot have special characters and cannot be empty. But this popup does not go away and ...

Announcement

We’re moving the ST Community to a new platform to give you a better and more reliable community experience.