2023-04-03 11:45 AM
I downloaded Cube Power Monitor and am trying to use it to connect to the LPM01A. I have downloaded and installed the W8 version of the virtual com port driver.
I can select the board in the drop down menu, but when I hit "Take Control", a dialog box pops up with the message `error pwr get`. When I hit okay, another pops up with the message `Get current range command failed` with another message below it `ERROR TIMEOUT`. Hitting ok again gives yet another dialog box with the message `Board has been released due to connection issue. Please unplug and plug the board`.
I've tried unplugging and plugging it back in and the same thing happens. I am currently on Windows 11, but I've tried on a different windows 10 machine and the result was exactly the same.
Any help would be appreciated.
Please also take a look at my other question for something that might be related... having lots of issues with this board so far...
Solved! Go to Solution.
2023-04-28 1:03 PM
I confirm it works now on Ubuntu 22.04 with 1.2.0 after updating the lpm01a board (from 1.0.1) to 1.0.8 (the latest at the time of writing).
2023-04-03 2:21 PM
Figured out a solution...
If I use version 1.1.1 instead of 1.2.0, then it works ... :expressionless_face:
2023-04-06 1:04 AM
@PDEFO.1, can you have a look
2023-04-06 1:12 AM
Thanks for your question. This issue was not reported before and not observed during validation tests.
For such issue it would be helpfull to get a log. Logs of the tool is located here :
C:\Users\<username>\AppData\Local\Temp\Power_Monitor\Logs
2023-04-10 4:50 AM
Same behaviour
2023-04-26 12:23 PM
I have the same error 1.2.0 fails on Windows 10, MacOs and Ubuntu 22.04.
Downgrading to 1.1.1 also fixed the issue for me.
Thank you ADing.1 for finding this solution!
2023-04-26 12:24 PM
Where can I find the logs on Ubuntu 22.04?
2023-04-27 12:27 AM
Logs for Linux are located In the "java temp directory"/powermonitor
2023-04-28 1:01 PM
I've upgraded the lpm01a board from version 1.0.1 to 1.0.8. Now both version 1.1.1 and 1.2.0 work on Ubuntu 22.04.
2023-04-28 1:03 PM
I confirm it works now on Ubuntu 22.04 with 1.2.0 after updating the lpm01a board (from 1.0.1) to 1.0.8 (the latest at the time of writing).
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.