STM32CubeMonitor (MCUs)

Ask questions on STM32CubeMonitor. Discuss the latest updates, including specialized versions (power, RF, USB-PD).

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

STM32CubeMonitor-1.12.0 is available

Hello The version 1.12.0 of STM32CubeMonitor is available on st.com :  https://www.st.com/en/development-tools/stm32cubemonitor.html What are the main changes in this version ? Node-RED® updated to version 4.1.3.STM32 devices list updated.Software de...

STM32CubeMonitor-RF V2.19.0 is available

Hello A new release of STM32CubeMonitor-RF is available on st.com. Click on "Get latest" to download the version 2.19.0. What are the main changes in this version ? Alignment with STM32CubeWB firmware 1.24.0.Alignment with STM32CubeWBA firmware 1.8.0...

Resolved! STLINK-V3PWR API

I've started using the recently published UM3291 to have smoother workflows with my other acquisition tools There are a few glitches that makes life a little bit more annoying than it should be.- The first one beeing the prompt "stlp >", which has to...

PMZ by Associate III
  • 8618 Views
  • 12 replies
  • 2 kudos

STM32CubeMonitor-Power Initial window size

When I open STM32CubeMonitor-Power (V1.2.1) the initial window is too large and spans both of my screens.My setup is HP Evny 17 laptop - Windows 11 (home) with 4K screen (3840x2160), secondary monitor full HD (1920x1080).Fortunately I can still acces...

SJame.1 by Associate II
  • 2191 Views
  • 2 replies
  • 0 kudos

STM32 Cube Monitor writing to a memory address

I am trying to write to a memory location for a nucleo board. As far as I have seen so far the simplest way to do this is as follows: This can be problematic when the code changes and the memory address shifts for the variable I'm interested. I'm su...

dq153252_0-1716558520791.png
dq153252 by Associate
  • 1450 Views
  • 1 replies
  • 0 kudos

Resolved! STM32CubeMonitor size of chart in dashboard

Hi,I use CubeMonitor V1.8.0 with my STM32G474QET device. Unfortunately the chart inside the dashboard is very small so I can`t work with it. Is there any possibility to set the size of the graph? The only thing I found is the duration in seconds, but...

berait by Associate III
  • 2022 Views
  • 2 replies
  • 0 kudos

Resolved! STM32CubeMonitor 1.8.0: no probe detected

I need to start using STM32CubeMonitor on my NUCLEO-G071RB to monitor some variables of my new firmware application developed with STM32CubeIDE 1.15.0. I never used STM32CubeMonitor before, so I installed the last STM32CubeMonitor 1.8.0 on my Windows...

Screenshot 2024-04-03 154704.png Screenshot 2024-04-03 155611.png Screenshot 2024-04-03 160253.png Screenshot 2024-04-03 160951.png
Vagni by Associate III
  • 2773 Views
  • 2 replies
  • 0 kudos

Is STM32CubeMonitor avilable to download?

I remember using this software about year ago, but I cant even download it.  https://www.st.com/en/development-tools/stm32cubemonitor.html#overview Ther is not any download link visible, but I see links and can download any other software.  I also ca...

Puchacz by Associate
  • 1337 Views
  • 1 replies
  • 0 kudos

ULP Bench Firmware for STM32CubeMonPwr

In the user manual for STM32CubeMonPwr it mentions the ability to run ULPMark tests. Where is the firmware located for running this benchmark? The link in the user manual goes to www.st.com (see section 4.8.2 above Figure 29)

rtswan22 by Associate
  • 1155 Views
  • 1 replies
  • 0 kudos

Monitor large structure in flash using STM32CubeMonitor

Hi everyone,I'm looking for a way to monitor a large structure using STM32CubeMonitor (or other solutions if not possible with CubeMonitor).I'm working on STM32L431RCT6My structure is composed like followed:typedef struct { uint16_t a; uint16_t b...

ijico by Associate
  • 1222 Views
  • 1 replies
  • 0 kudos