STM32CubeMonitor (MCUs)

Ask questions on STM32CubeMonitor. Discuss the latest updates, including specialized versions (power, RF, USB-PD).

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

STM32CubeMonitor-1.12.0 is available

Hello The version 1.12.0 of STM32CubeMonitor is available on st.com :  https://www.st.com/en/development-tools/stm32cubemonitor.html What are the main changes in this version ? Node-RED® updated to version 4.1.3.STM32 devices list updated.Software de...

STM32CubeMonitor-RF V2.19.0 is available

Hello A new release of STM32CubeMonitor-RF is available on st.com. Click on "Get latest" to download the version 2.19.0. What are the main changes in this version ? Alignment with STM32CubeWB firmware 1.24.0.Alignment with STM32CubeWBA firmware 1.8.0...

Resolved! Professional STM32 Embedded Systems Testing Setup

Recently I have been tasked with developing our companies embedded testing strategy. The task is little bit above me since this is my first job, however I am determined to learn anything I need to and put together a solution that works for the compan...

Ahmed by Associate III
  • 2709 Views
  • 1 replies
  • 0 kudos

Resolved! How to write a float with a slider

howdy,I'm using this setup: https://community.st.com/s/question/0D53W000005571h/how-to-write-variable-from-flow-in-cubemonitorto write values with a slider, but it doesn't seem to work with a float.1: what do the numbers in the "type" field actually ...

Resolved! How can I run the dashboard on IOS

I'd like to run the dashboard on my iphone. I'm able to run it in Chrome on my mac with no problems, but am missing something about how to get this to work on my phone. Any help is appreciated!

Resolved! On a Mac, "paste" does not seem to work.

I'm on a Mac, and CMD+V does not seem to work for paste. I'm not able to copy or paste any text from within or from outside into cube monitor. this makes some things pretty tedious! any idea what this is about?

Resolved! elf parser seems not working properly

After loading the elf file variables are detected incorrect (wrong address an/or size)Two examples with output of readelf1) used in *.c file:uint8_t counter_error_handler __attribute__((section(".internal_ram")));> readelf Bluepill_USB_CDC.elf -s |gr...

0693W000006GuTKQA0.png

Resolved! How can i manage projects

Hello, lets say i have more than one project in a lifetime. How can i use CubeMonitor to use different Projects? Its very weired that all flows are linked together in any way. Why is it not as the old tool STM Studio, there you can create a own proje...

Resolved! STM32CubeMonitor F.A.Q.

HelloThe frequent questions for Cube Monitor have been listed on a wiki page :https://wiki.st.com/stm32mcu/wiki/STM32CubeMonitor:Frequently_Asked_QuestionsWe have already included some questions from the webinars and we will continue to add new quest...

Resolved! STM32CubeMonitor-RF V2.6.0 released

New version 2.6.0 is released.New features : Some 802.15.4 RF tests are added to make certification tests easier : In the transmitter test,it is possible to send MAC frames . The frame can be defined by the user. In the receiver test, the LQI, ED, a...