STM32CubeMonitor (MCUs)

Ask questions on STM32CubeMonitor. Discuss the latest updates, including specialized versions (power, RF, USB-PD).

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

STM32CubeMonitor-1.12.0 is available

Hello The version 1.12.0 of STM32CubeMonitor is available on st.com :  https://www.st.com/en/development-tools/stm32cubemonitor.html What are the main changes in this version ? Node-RED® updated to version 4.1.3.STM32 devices list updated.Software de...

STM32CubeMonitor-RF V2.19.0 is available

Hello A new release of STM32CubeMonitor-RF is available on st.com. Click on "Get latest" to download the version 2.19.0. What are the main changes in this version ? Alignment with STM32CubeWB firmware 1.24.0.Alignment with STM32CubeWBA firmware 1.8.0...

Resolved! STM32CubeMonitor: reading from a serial port

Hi,first I want to say that STM32CubeMonitor (I am running 1.1.0) is a really fantastic debug tool, and it was a really good idea from ST do use nodered for this.It makes many debug tasks A LOT easier than before and it is really a lot of fun to play...

papamidas by Associate II
  • 5787 Views
  • 6 replies
  • 0 kudos

Resolved! Monitoring variables in a table in CubeMonitor

Hi, I need to monitor variables from my program in CubeMonitor. I was able to follow a few videos from Youtube and set up the values in a chart. However, that is a very clunky interface. Please note that I have zero experience with nodered.

Resolved! How can i round the digits of a number?

Hi,i am new with node-red functionality and i want to decrease the digits in a Gauge.When i start the Dashboard i get the temperature in e.g. 21.77615442345 degrees. And i want to show it with 2 digits e.g. 21.78 degrees.Ho can i do this?

ledi001 by Senior
  • 5834 Views
  • 2 replies
  • 0 kudos

Resolved! Monitoring an array in STM32CubeMonitor

This might seem like a noob Q but how can I monitor an array in Cube Monitor? I find it really confusing and as the screen shot below shows, I can only see the 0th element of the array but not the others. Am I missing something?

0693W000007Dng0QAC.png

Resolved! STM32CubeMonitor display multiple variables

Dear all,I used STMStudio until today to watch multiples values in real time.Today i want to use STM32CubeMonitor and it seems a very interesting tool.However i don't find a quick way to visualize multiple variables values in a array like STMstudio a...

0693W000007DEOLQA4.png 0693W000007DEQWQA4.png
FGERM.11 by Associate II
  • 2947 Views
  • 5 replies
  • 0 kudos

Resolved! How to get *.out file?

Hi, When i use STM32CubeMonitor, I can't understand add some of values.*.out file is not created when stm32 project debug?​How to get this file or know value's start address?

0693W000007AqQxQAK.png 0693W000007AqR7QAK.png

Resolved! Application server port already in use

When starting STM32CubeMonitor it displays a dialog reporting "Application server port already in use"; the application then exits when the dialog is closed.In the details it says that port 1880 is already in use; however netstat doesn't show this po...