STM32CubeMonitor (MCUs)

Ask questions on STM32CubeMonitor. Discuss the latest updates, including specialized versions (power, RF, USB-PD).

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

STM32CubeMonitor-1.12.0 is available

Hello The version 1.12.0 of STM32CubeMonitor is available on st.com :  https://www.st.com/en/development-tools/stm32cubemonitor.html What are the main changes in this version ? Node-RED® updated to version 4.1.3.STM32 devices list updated.Software de...

STM32CubeMonitor-RF V2.19.0 is available

Hello A new release of STM32CubeMonitor-RF is available on st.com. Click on "Get latest" to download the version 2.19.0. What are the main changes in this version ? Alignment with STM32CubeWB firmware 1.24.0.Alignment with STM32CubeWBA firmware 1.8.0...

STM32CubeMonitor-Power Feature Request

Hello,the STM32CubeMonitor-Power is a very useful tool and I am using it a lot.For power optimizing applications often the period, at which current pulses occur, help a lot to find the source. Therefore I am missing a "Cursor" feature for this tool.W...

c_dev05 by Associate III
  • 1729 Views
  • 2 replies
  • 3 kudos

Resolved! Missing acquisition nodes on macOS

Hello,Today I tried using STM32CubeMonitor 1.7.0 on macOS Sonoma (MacBook with M1 chip), but after installing the app opens without acq in and acq out nodes in the library, and of course it complains about missing node types when loading sample Basic...

Jabub by Associate
  • 3006 Views
  • 2 replies
  • 1 kudos

Resolved! Cannot read voltage measurement inside UCPD monitor

I have followed this STM wiki tutorial about basic PD Sink. Everything is running according to it, but I am unable to see voltage and current measurement inside UCPD monitor. I have also followed the set-up of debugging button which is working correc...

Marosh by Associate III
  • 2709 Views
  • 3 replies
  • 2 kudos

Resolved! Is STM32CubeMonitor a standalone application?

Hello, from what I read in the ST wiki I understand that the STM32CubeMonitor (MON) is a standalone application? A P2P connection to the 'probe' (e.g. the ST-LINK/V2) is used in this configuration.That means: it is not required that the STM32CubeIDE ...

Kmax18 by Senior II
  • 1543 Views
  • 1 replies
  • 1 kudos

Resolved! X-NUCLEO-LPM01A installation issue

Hi!I'm having problem connecting the board to a Windows 10 PC. Connecting the board to the USB it works in standalone mode, but the USB driver (PowerShield Virtual ComPort in FS Mode) is not installed, so I can't use the board with the STM32CubeMonit...

paolog by Senior
  • 1426 Views
  • 1 replies
  • 0 kudos