2023-07-11 12:20 AM - edited 2023-07-12 2:13 AM
Something went wrong with the Energy Values in µJ yesterday.
If I am not mistaken, to go from µA to µJ should be voltage*current*seconds, so 2546µA average current for 2,052 seconds with 3,3V input voltage should be 17240µJ.
The monitor software said 1332,621µJ. I have no idea why.
A similar measurement after restarting this morning looks ok again:
Edit: A few minutes later it's broken again and even reconnecting the power meter and restarting the software does not help to recover again
2023-07-11 12:48 AM
Hi @OliM ,
You are right it looks like something wrong with the way STM32CubeMonitor-Power calculates the energy based on the measurement.
I will escalate this issue, please can you give me more information:
- Are you using the new STLINK-PWR ?
- Can you confirm that your are using the version v1.2.1?
Best regards,
Aime
2023-07-11 1:34 AM - edited 2023-07-11 1:35 AM
As you can see on the screenshots, I am using the STLINK-V3PWR at firmware V4J2B1P4 with the monitor version v1.2.1 . It feels in the moment like only the first measurement of the day is computed correctly. I have some other tasks to do because of which I can not restart my PC right now, but I will also try that some time later.
i have used the 1.1.x with the L5 disco with integrated power meter in the past and have not seen the issue there.
2023-07-11 1:58 AM
Hi @OliM ,
Thank you for your feedback, I escalated this to your Tools team.
We will check if the issue is due to the STLINK-PWR firmware or STM32CubeMonitor-PWR, and get back to you as soon as possible.
For now, can you try on the previous version of STM32CubeMonitor-PWR (v1.1.1) if you have the same issue? Please keep the STLINK-PWR for the trial.
Best regards,
Aime
2023-07-11 3:55 AM
v1.1.1 seems to be stable (but of course missing the power on/off switch of 1.2.1)
2023-07-25 6:26 AM
2024-01-11 3:40 AM
i have a similar issue with energy calculation:
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.