2024-01-12 9:52 AM
Hi!
I'm having problem connecting the board to a Windows 10 PC. Connecting the board to the USB it works in standalone mode, but the USB driver (PowerShield Virtual ComPort in FS Mode) is not installed, so I can't use the board with the STM32CubeMonitor-Power. Windows Device Manages tells that device drivers have not been installed, and the associated COM port is obviously not existing.
Is the X-NUCLEO-LPM01A not functioning properly or am I missing something?
Solved! Go to Solution.
2024-01-13 12:26 AM
Ok, I just needed to upgrade the firmware of the X-NUCLEO-LPM01A...
2024-01-13 12:26 AM
Ok, I just needed to upgrade the firmware of the X-NUCLEO-LPM01A...
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.