2021-05-02 9:56 AM
Dear all,
I am using stm32cubeide with stm32l4p5 micro.
Everything is working fine but for the first time, I try to write and read my USB key.
For that, i use the USB_OTG_FS set up
I am able to write and read only one time and the recorded file is OK
But the issue is, if I try to record several time in the while(1) loop, I get a HardFault_Handler() at stm32l4xx_it.c:90 0x800b2d2 and the program stop.
I saw some equivalent issues in the past, but I don't understand how to solve this issue.
Thanks for your help
Robert
2021-05-02 10:41 AM
Rather that have a while(1) loop in the Hard Fault Handler, unpack the fault state and look at what's actually faulting.
Invalid addresses/pointers, corrupt structures/instances, resource leaks on the heap
2021-05-03 2:02 AM
Dear Member,
Thanks for your answer.
Sorry, I was not clear. The while (1) is the loop of the main task.
Below is the detail of 2 version of this while (1)
PPROGRAM1 with N_Write_USB limiting use of MX_USB_HOST_Process() only ONE TIME, Recording is successfull;
PPROGRAM2 without N_Write_USB use of MX_USB_HOST_Process() MANY TIMES, Recording fail; I don't understand why ?
Best Regards
Robert
xxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxx
PPROGRAM1 with N_Write_USB
/* Infinite loop */
/* USER CODE BEGIN WHILE */
while (1)
{
#ifdef WRITE_USB
if(N_Write_USB == 0)
{
uint8_t i , j;
for ( i = 0 ; i < strlen(wrchar_text_USB) ; i ++) {wrchar_text_USB[i] = '\0'; }
for ( i = 0 ; i < strlen(char_file_USB) ; i ++) {char_file_USB[i] = '\0';}
//Programmation du Fichier
char_file_USB[0] = 'L';
char_file_USB[1] = 'I';
char_file_USB[2] = 'S';
char_file_USB[3] = 'T';
char_file_USB[4] = 'M';
char_file_USB[5] = 'O';
char_file_USB[6] = 'D';
char_file_USB[7] = '.';
char_file_USB[8] = 'T';
char_file_USB[9] = 'X';
char_file_USB[10] = 'T';
char_file_USB[11] = '\0';
//Programmation du Parametre
char result_2ascii[2];
// Autres Modeles
wrchar_text_USB[0] = '_';
_ByteTo_Result_2ascii(Model_Num[0], result_2ascii);
strcat(wrchar_text_USB, result_2ascii);
strcat(wrchar_text_USB, "_");
strcat(wrchar_text_USB, "x");
strcat(wrchar_text_USB, Model_Name[0]);
strcat(wrchar_text_USB, "x");
strcat(wrchar_text_USB, "_");
_ByteTo_Result_2ascii(Model_Num[1], result_2ascii);
strcat(wrchar_text_USB, result_2ascii);
strcat(wrchar_text_USB, "_");
strcat(wrchar_text_USB, "x");
strcat(wrchar_text_USB, Model_Name[1]);
strcat(wrchar_text_USB, "x");
Flag_Write_USB = TRUE;
HAL_Delay(100);
}
N_Write_USB++;
//
#endif //WRITE_USB
if((Flag_Write_USB==TRUE)||(Flag_Read_USB==TRUE)||(Flag_WriteRead_USB))
{
/* USER CODE END WHILE */
MX_USB_HOST_Process();
/* USER CODE BEGIN 3 */
} //End if((Flag_Write_USB==TRUE)||(Flag_Read_USB==TRUE)||(Flag_WriteRead_USB))
} //End while (1)
xxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxx
PPROGRAM2 without N_Write_USB
/* Infinite loop */
/* USER CODE BEGIN WHILE */
while (1)
{
#ifdef WRITE_USB
//// if(N_Write_USB == 0)
//// {
uint8_t i , j;
for ( i = 0 ; i < strlen(wrchar_text_USB) ; i ++) {wrchar_text_USB[i] = '\0'; }
for ( i = 0 ; i < strlen(char_file_USB) ; i ++) {char_file_USB[i] = '\0';}
//Programmation du Fichier
char_file_USB[0] = 'L';
char_file_USB[1] = 'I';
char_file_USB[2] = 'S';
char_file_USB[3] = 'T';
char_file_USB[4] = 'M';
char_file_USB[5] = 'O';
char_file_USB[6] = 'D';
char_file_USB[7] = '.';
char_file_USB[8] = 'T';
char_file_USB[9] = 'X';
char_file_USB[10] = 'T';
char_file_USB[11] = '\0';
//Programmation du Parametre
char result_2ascii[2];
// Autres Modeles
wrchar_text_USB[0] = '_';
_ByteTo_Result_2ascii(Model_Num[0], result_2ascii);
strcat(wrchar_text_USB, result_2ascii);
strcat(wrchar_text_USB, "_");
strcat(wrchar_text_USB, "x");
strcat(wrchar_text_USB, Model_Name[0]);
strcat(wrchar_text_USB, "x");
strcat(wrchar_text_USB, "_");
_ByteTo_Result_2ascii(Model_Num[1], result_2ascii);
strcat(wrchar_text_USB, result_2ascii);
strcat(wrchar_text_USB, "_");
strcat(wrchar_text_USB, "x");
strcat(wrchar_text_USB, Model_Name[1]);
strcat(wrchar_text_USB, "x");
Flag_Write_USB = TRUE;
HAL_Delay(100);
////// }
////N_Write_USB++;
#endif //WRITE_USB
if((Flag_Write_USB==TRUE)||(Flag_Read_USB==TRUE)||(Flag_WriteRead_USB))
{
/* USER CODE END WHILE */
MX_USB_HOST_Process();
/* USER CODE BEGIN 3 */
} //End if((Flag_Write_USB==TRUE)||(Flag_Read_USB==TRUE)||(Flag_WriteRead_USB))
} //End while (1)
2021-05-03 2:43 AM
As Clive said, observe in the fault handler, where the fault happened, and in mixed source/debug view find, which instruction caused the problem (you may need to go backwards a couple of instructions). Observe content of registers and match them to the variables in source. That will help you find the source of problem.
In other words, only in rare cases (when there's a widely used code with a known straightforward bug) the problem can be deciphered by looking at a fragment of source code which uses a bunch of deep and complex function calls and unknown data and structures. It's up to you to drill down. That you used some clicky configurator and a prechewed "library", that's your problem.
JW
2021-05-05 12:08 AM
Thanks Jan for your reply,
I will try to understand this.
I was expecting a more obvious mistake in my software for the USB key. (Above)
Best Regards
Robert
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.