2025-02-16 10:21 AM
Hi.
I am using TouchGFX and it works fine,
My MCU is STM32H743
But when I use the SDRAM for other things the code does not work.
My question is:
Can I use struct in the SDRAM.?
I have this one in my c file.
SD_CARD SdCard __attribute__((section("\"SDCardSection\""))) __attribute__((aligned(4)));
In my h file as follows:
typedef struct {
char Name[256];
char Path[1000];
char File[2000];
uint8_t LogicalDrive;
}SD_CARD;
extern SD_CARD SdCard __attribute__((section("\"SDCardSection\""))) __attribute__((aligned(4)));
My Linker file is as follows:
/* Entry Point */
ENTRY(Reset_Handler)
/* Highest address of the user mode stack */
_estack = ORIGIN(RAM_D1) + LENGTH(RAM_D1); /* end of RAM */
/* Generate a link error if heap and stack don't fit into RAM */
_Min_Heap_Size = 0x400; /* required amount of heap */
_Min_Stack_Size = 0x800; /* required amount of stack */
/* Specify the memory areas */
MEMORY
{
FLASH (rx) : ORIGIN = 0x08000000, LENGTH = 2048K
DTCMRAM (xrw) : ORIGIN = 0x20000000, LENGTH = 128K
RAM_D1 (xrw) : ORIGIN = 0x24000000, LENGTH = 512K
RAM_D2 (xrw) : ORIGIN = 0x30000000, LENGTH = 288K
RAM_D3 (xrw) : ORIGIN = 0x38000000, LENGTH = 64K
ITCMRAM (xrw) : ORIGIN = 0x00000000, LENGTH = 64K
QUADSPI (r) : ORIGIN = 0x90000000, LENGTH = 16M
SDRAM (xrw) : ORIGIN = 0xC0000000, LENGTH = 32M
}
etc
etc
etc
.ARM.attributes 0 : { *(.ARM.attributes) }
BufferSection (NOLOAD) :
{
*(Video_RGB_Buffer Video_RGB_Buffer.*)
*(.gnu.linkonce.r.*)
. = ALIGN(0x4);
*(TouchGFX_Framebuffer TouchGFX_Framebuffer.*)
*(.gnu.linkonce.r.*)
. = ALIGN(0x4);
} >SDRAM
SDCardSection (NOLOAD) :
{
*(SDCardSection SDCardSection .*)
*(.gnu.linkonce.r.*)
. = ALIGN(0x4);
} >SDRAM
Best Regards.
Solved! Go to Solution.
2025-02-25 9:06 AM
Hi there.
The problem was that TouchGFX uses Unicode.
I was using char buffer and pointers to update the buffer of a scrollWheel.
But TouchGFX describes that we should use the Unicode library.
So, I updated my buffers to datatype uint16_t, and then used the Unicode library.
void CustomContainer2_1::UpdateText(uint16_t value)
{
Unicode::snprintf(textArea1Buffer, TEXTAREA1_SIZE, "%s", &SdCard.File);
...
...
...
...
textArea1.invalidate();
}
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.