2021-01-01 3:11 PM
I get the following error in terminal quite frequently which crashes the stm32cubeide. This usually happens when I am opening the ".ioc" file.
Attempt to unlock mutex that was not lockedThis is my workspace folder if you are interested: https://github.com/yosoufe/ExperineceKemet/tree/master/cubews
I also sometimes see the following error message and then a crash
[xcb] Unknown sequence number while processing reply
[xcb] Most likely this is a multi-threaded client and XInitThreads has not been called
[xcb] Aborting, sorry about that.
java: ../../src/xcb_io.c:639: _XReply: Assertion `!xcb_xlib_threads_sequence_lost' failed.I should run it via terminal to see the error. If I click on the icon, it crashes without any error message.
I am running it on Ubuntu 18.04 machine. Is there anyway to run the cubeIDE in safe mode to disable some plugins?
Thanks
2021-07-31 11:36 PM
Same here, release 1.7.0 and Cube keeps randomly crashing (way worse than previous releases), making it barely usable just for templates generation.
2021-08-01 12:20 AM
@YEbne.1 @DFedo.1 googling a bit sounds like GTK issue. Which GTK version are you relying on ?
Are you relying on Xorg or Wayland ?
2021-08-01 5:34 AM
libgtk-3, up to date ubuntu 20.04 LTS, xorg
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.