STM32CubeIDE (MCUs)

Ask questions on STM32CubeIDE. Discuss how to build, debug, configure, and optimize your project as well as how to use our software tools.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

STM32CubeIDE 2.1.1 released

We are pleased to announce that the minor version 2.1.1 of STM32CubeIDE is available. What is new in 2.1.1: This release covers the topics listed below: SEGGER J-Link GDB server updated to 9.24 to fix an issue with the Live Expression view during the...

Aimen1 by ST Employee
  • 1703 Views
  • 0 replies
  • 1 kudos

STM32CubeCLT 1.21.0 released

We are pleased to announce that STM32CubeCLT 1.21.0 release is available. What is new in 1.21.0: Maintenance of the previous version: Updated in accordance with STM32CubeIDE v2.1.0Update of Clang/LLVM toolchainUpdate of GCC to GCC 14Update of STM32Cu...

Aimen1 by ST Employee
  • 638 Views
  • 0 replies
  • 0 kudos

STM32CubeIDE 2.0 release - early heads-up!

Starting from the release in November 2025, STM32CubeIDE and STM32CubeMX will be available exclusively in their standalone versions. STM32CubeMX will no longer be integrated inside STM32CubeIDE. Instead, the two tools will be interoperable in the sam...

Hello- New to ST32 and the IDE, and re-learning C as well. I am trying to work an example using I2C for a 2 line by 16 digit LCD. When I compile (build) I get 4 errors, need to help if you would. 1st time poster....

error: 'for' loop initial declarations are only allowed in C99 or C11 mode 223 |  for(uint8_t i=0; i<offset;i++) error: 'for' loop initial declarations are only allowed in C99 or C11 mode 234 |  for(uint8_t i=0; i<offset;i++)error: 'for' loop initial...

SScot.3 by Associate II
  • 1725 Views
  • 3 replies
  • 0 kudos

Filed to start GDB server

I am using two NUCLEO-H745ZI-Q board . I want two debug window at time.Because i want loopbacking of spi. One board is work as MASTER and another board is worked as SLAVE. Master file is open from STMcubeIDE 1.6.1 version and slave project file ope...

0693W00000D10gLQAR.png 0693W00000D10hdQAB.png 0693W00000D10hYQAR.png 0693W00000D10hTQAR.png
MDeva.1 by Associate II
  • 848 Views
  • 0 replies
  • 0 kudos

Resolved! STM32F733xx SPI DMA transfer issue.

I've built a custom system using the STM32F733xx and an external ADC (TI ADS8588S) connected over SPI. I have verified that the system works consistently using the STM32 HAL L0_V1.2.8 when transferring data via the blocking/polling method. However, w...

0693W00000AOPZnQAP.png
Grundyoso by Associate II
  • 3927 Views
  • 6 replies
  • 0 kudos

Resolved! Is there a way to set argc/argv when remote debugging?

Some remote debugging tools (Arm's DS-5 semihosting) allow setting arguments to main(). I'm unable to figure out the steps do this with stlink + gdb remote targeting because it doesn't support "run", only "continue". Is there a way to do this with a ...

Resolved! CubeIDE cannot clean project

I've just now switched from TrueSTUDIO to CubeIDE 1.7.0, and when I tried to clean the project by selecting Project -> Clean ... from the menu, I got an error message:19:26:52 **** Clean-only build of configuration Debug for project xx **** make clea...

Announcement

We’re moving the ST Community to a new platform to give you a better and more reliable community experience.