cancel
Showing results for 
Search instead for 
Did you mean: 

Multiline selection not visible after MacOS 26.2 update

snigg
Associate III

It seems that after I updated MacOS to Tahoe 26.2 the IDE does not show selected text if over multiples lines correctly. This is a nightmare to work with, as it does not show selected text and can make you delete (overwrite) lines while editing.
Anyone else? Is there a setting to fix it?

12 REPLIES 12
Ghofrane GSOURI
ST Employee

Hello @snigg 

Thank you for posting.

A ticket has been escalated to dev team regarding this issue.

Internal ticket ID is 224479 and it will be fixed as soon as possible.

THX

Ghofrane

To give better visibility on the answered topics, please click on Accept as Solution on the reply which solved your issue or answered your question.

snigg
Associate III

Any update on this? I have seen with the ticket ID this already has been raised last year. It is very annoying to use the IDE this way.

Hello @snigg 

Yes, I agree with you that this issue is very annoying. However, macOS 12.6.2 was published on December 12, 2025
(link: https://developer.apple.com/news/releases/?id=12122025c).

STM32CubeIDE 2.0.0 was released on November 18, 2025, and the ticket was escalated on 2025-12-30. We are doing our best to correct this behavior as soon as possible.

THX

Ghofrane

To give better visibility on the answered topics, please click on Accept as Solution on the reply which solved your issue or answered your question.

Its been more than a week and there is still no update. What is the timeline?!

snigg
Associate III

ST, please take down the note you support MacOS and or set STM32CubeIDE to legacy status. You seemed to have invested in a Visual Code Studio integration of the STM32 stuff, so is this now the way to go? Could you at the very least be transparent in your strategy?!

Arete
Associate II

Same issue here, please provide update.  Frustrating to say the least.

So, I just installed 2.1 just to realise you DID NOT fix the issue! Are you f*** kidding me!

Nick_Art
Associate II

It is really annoying - frustrating.

 

I also filed a ticket. Lets hope they will fix it. Or otherwise I'll buy other microcontroller from a different manufacturer.

VSCode does not have the nicer debug facility. 

SJB
Associate

Five months later and it's still not fixed. STM32CubeIDE v2.1.1.  MacOS Tahoe 26.3.1  Extremely frustrating. As it cripple all but simple code editing.

As we don't have access to Internal ticket ID 224479 could someone at ST give us an update please, and confirm the statement made in January that "it will be fixed as soon as possible" (that statement is feeling a little hollow now).

Or, is STM32CubeIDE moving rapidly towards being considered legacy, as that's what it feels like, given the crippling nature of this bug and lack of any fix for so long.