cancel
Showing results for 
Search instead for 
Did you mean: 

Error downloading the following files: api_config.json (Not Available)

Marvin_k
Associate

This error pops up everytime I try creating a new STM32 project when downloading the selected files during the first stages of creating a project. My internet connection is fine and this wasn't an issue some weeks back with the last project I created. Any assistance on this issue from anyone will be very helpful because I'm a quite a newbie to CubeIDE. Thanks.

1 ACCEPTED SOLUTION

Accepted Solutions
Adison112
Associate

I think this problem is caused by new update. I've been working in Cube for several years but I've never updated the software. After replacing CubeMX with newer it works fine. 

View solution in original post

9 REPLIES 9
amirkfir
Associate II

Having the same issue

Adison112
Associate

Same to me

 

nsacut
Associate

same here

Adison112
Associate

I think this problem is caused by new update. I've been working in Cube for several years but I've never updated the software. After replacing CubeMX with newer it works fine. 

AA6
Associate II

Same problem, happens also with creating new project from existing .ioc file. After the download fails project creation menu appears but IDE gets stuck in Progress Information tab and nothing is clickable. I'm using CubeIDE v1.19.

AA6
Associate II

Quick update: When I did not click OK to api_config.json error it disappeared on its own and I was able to create a project. Then I downloaded firmware packages I needed from MX UI (manage software packages)

I was still able to build my project and flash the MCU after clicking the box away, so it didn't end up really interfering this time. I feel that I'll eventually run into some project that'll need those missing files though. Anyway, I also haven't updated my CubeIDE so that might be it. 

Atharv21
Associate

Same here 

Ldy216
Associate

Same here ,while downloading