2022-12-01 2:41 AM
Hi Coders,
i have added a library trough linked folders (Source location-> Link Folder..) where most of my code is in that i want to re-use in several projects.
But often i see that type's generated by the code generator (ioc) are not "seen" by my library.
The library is not compiled but exist of many c and header files.
To give a clear example :
Some main projects use the DAC, when i activate DAC in ioc, i get type DAC_HandleTypeDef to use in my main project.
In my library i have added code to create a member when DAC_HandleTypeDef exists like this :
#ifdef DAC_HandleTypeDef
DAC_HandleTypeDef *pDAC_Speed;
#endifThis does not work, the libary code thinks the DAC_HandleTypeDef is not defined while i can use DAC_HandleTypeDef type in my mainproject.
I did follow the header sequence , and see that DAC_HandleTypeDef is defined trough "stm32g4xx_hal.h" which is the very first header in the main project. While my library headers should be compiled later.
What's going on?
How do you guys/girls solve this issue?
Thank you
Solved! Go to Solution.
2022-12-01 10:55 AM
DAC_HandleTypeDef is a defined type (typedef struct ...). This is different to a defined preprocessor macro what you are testing for with #ifdef. There is no standard way in C to test wether a type exists or not.
What you could do, you could check wether the entire DAC module is included in your project with
#ifdef HAL_DAC_MODULE_ENABLEDdefined (or not defined) in stm32g4xx_hal_conf.h
hth
KnarfB
2022-12-01 10:55 AM
DAC_HandleTypeDef is a defined type (typedef struct ...). This is different to a defined preprocessor macro what you are testing for with #ifdef. There is no standard way in C to test wether a type exists or not.
What you could do, you could check wether the entire DAC module is included in your project with
#ifdef HAL_DAC_MODULE_ENABLEDdefined (or not defined) in stm32g4xx_hal_conf.h
hth
KnarfB
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.