STM32CubeIDE (MCUs)

Ask questions on STM32CubeIDE. Discuss how to build, debug, configure, and optimize your project as well as how to use our software tools.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

STM32CubeIDE 2.1.1 released

We are pleased to announce that the minor version 2.1.1 of STM32CubeIDE is available. What is new in 2.1.1: This release covers the topics listed below: SEGGER J-Link GDB server updated to 9.24 to fix an issue with the Live Expression view during the...

Aimen1 by ST Employee
  • 1703 Views
  • 0 replies
  • 1 kudos

STM32CubeCLT 1.21.0 released

We are pleased to announce that STM32CubeCLT 1.21.0 release is available. What is new in 1.21.0: Maintenance of the previous version: Updated in accordance with STM32CubeIDE v2.1.0Update of Clang/LLVM toolchainUpdate of GCC to GCC 14Update of STM32Cu...

Aimen1 by ST Employee
  • 638 Views
  • 0 replies
  • 0 kudos

STM32CubeIDE 2.0 release - early heads-up!

Starting from the release in November 2025, STM32CubeIDE and STM32CubeMX will be available exclusively in their standalone versions. STM32CubeMX will no longer be integrated inside STM32CubeIDE. Instead, the two tools will be interoperable in the sam...

STM32G031J6, STlink not detected

I am new to STM32 programming and while using cubeIde to work on led blinking project. The project is built successfully but after this I get an error that No target found. This happens eventhough I have plugged in the board. So, do I need to use a e...

AZadb.1 by Associate II
  • 4098 Views
  • 9 replies
  • 0 kudos

setting A15 in GPIOA->ODR (STM32F103C8T6)

I'm pulling my hair because in a GPIO->ODR = 0x7fff bit A15 is not going down to 0. At least cannot trigger it with the negative slope in pulseview/ (sigrok FX2 LA).A0-A3 are already programmed as outputs. This is the code in STM32CubeIDE:static void...

Project migration from different laptop

Hi,We meet an issue concerning a project migration from a laptop to an another.Build systematic fail during build, we try to :Import project from folder through IDE interface.Clean project before buildCompiler found errors : c:\st\stm32cubeide_1.7.0\...

BKOSI.1 by Associate II
  • 6009 Views
  • 10 replies
  • 0 kudos

Using St Cube IDE 1.6.0, I create new project for STM32F302C8. When debugging the project i noticed that my HSE crystal is not working (Systick is always 0). The code ends up in an infinite loop which prevents the HSE. Who can help me ??

/* USER CODE BEGIN Header *//**  ******************************************************************************  * @file           : main.c  * @brief          : Main program body  **********************************************************************...

jvan .1 by Associate II
  • 1697 Views
  • 3 replies
  • 0 kudos

Build fail since CubeIDE update to 10.1

Hi,I'm looking for a support concerning a STM32U585 firmware.After an update of CubeIDE, build fail with this errror :09:43:17 **** Build of configuration Debug for project BlackBox ****make -j8 all Middlewares/BlackBox_Manager/Src/main_manager.d:130...

BKOSI.1 by Associate II
  • 6550 Views
  • 9 replies
  • 0 kudos
Announcement

We’re moving the ST Community to a new platform to give you a better and more reliable community experience.