2021-03-04 9:07 AM
I’m very new to STM32 development so bear with me if this is a simple question. I’m trying to use an L476RG Nucleo and X-Nucleo-ihm03a1 powerSTEP01 board to control stepper motors.I’ve downloaded X-CUBE-SPN3 Driver software expansion for STM32Cube and have skimmed the following manual
the example projects only support toolchains EWARM, MDK-ARM and SW4STM32. Theres a number of files that came with the X-CUBE-SPN3 download, which files are the right driver files and how do I import them into an STMCUBEIDE project?
Solved! Go to Solution.
2021-03-10 6:41 AM
Hello @ZHama.1 and welcome to the ST Community.
I confirm: the SW4STM32 - System Workbench toolchain - is compliant with STM32CubeIDE.
The X-CUBE-SPN3 is compatible with the NUCLEO-F401RE, NUCLEO-F030R8, NUCLEO-F334R8 and NUCLEO-L053R8 boards.
I suggest to import one of available projects and make changes according your STM32 part number (NUCLEO-L476RG with STM32L476RG).
The path is ...\STM32CubeExpansion_SPN3_V1.6.0\Projects\Multi\Examples\MotionControl\IHM03A1_ExampleFor1Motor\SW4STM32
(if you want to drive a single motor otherwise you can choose IHM03A1_ExampleFor2Motor or IHM03A1_ExampleFor3Motor).
Let me know if these info are useful to you, if yes please "Select as Best" button to close the topic.
2021-03-04 9:14 AM
Rely on SW4STM32 data which are STM32CubeIDE compliant.
If STM32CubeIDE just rely on File > Open Project From File System. Provide path up to SW4STM32 folder at min (next level - most probably target device name - is even better)
2021-03-10 6:41 AM
Hello @ZHama.1 and welcome to the ST Community.
I confirm: the SW4STM32 - System Workbench toolchain - is compliant with STM32CubeIDE.
The X-CUBE-SPN3 is compatible with the NUCLEO-F401RE, NUCLEO-F030R8, NUCLEO-F334R8 and NUCLEO-L053R8 boards.
I suggest to import one of available projects and make changes according your STM32 part number (NUCLEO-L476RG with STM32L476RG).
The path is ...\STM32CubeExpansion_SPN3_V1.6.0\Projects\Multi\Examples\MotionControl\IHM03A1_ExampleFor1Motor\SW4STM32
(if you want to drive a single motor otherwise you can choose IHM03A1_ExampleFor2Motor or IHM03A1_ExampleFor3Motor).
Let me know if these info are useful to you, if yes please "Select as Best" button to close the topic.
2021-03-22 2:27 AM
Hi @ZHama.1 ,
any news about your project progress?
2021-03-27 8:22 AM
Ha yes, looking back this question is ridculously straight forward.
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.