2023-04-04 2:33 AM
#include "main.h"
#include "vl53l0x_i2c_platform.h"
#include "vl53l0x_api.h"
#include "vl53l0x_platform.h"
#include "vl53l0x_platform_log.h"
I2C_HandleTypeDef hi2c1;
RTC_HandleTypeDef hrtc;
/* Private function prototypes -----------------------------------------------*/
void SystemClock_Config(void);
static void MX_GPIO_Init(void);
static void MX_I2C1_Init(void);
static void MX_RTC_Init(void);
/* USER CODE BEGIN PFP */
/* USER CODE END PFP */
/* Private user code ---------------------------------------------------------*/
/* USER CODE BEGIN 0 */
/* USER CODE END 0 */
/**
* @brief The application entry point.
* @retval int
*/
int main(void)
{
uint8_t buff =0;
VL53L0X_Error Status = VL53L0X_ERROR_NONE;
VL53L0X_Dev_t MyDevice;
VL53L0X_Dev_t *pMyDevice = &MyDevice;
VL53L0X_Version_t Version;
VL53L0X_Version_t *pVersion = &Version;
VL53L0X_DeviceInfo_t DeviceInfo;
pMyDevice->I2cDevAddr = 0x52;
pMyDevice->comms_type = 1;
pMyDevice->comms_speed_khz = 400;
/* USER CODE BEGIN 1 */
/* USER CODE END 1 */
/* MCU Configuration--------------------------------------------------------*/
/* Reset of all peripherals, Initializes the Flash interface and the Systick. */
HAL_Init();
/* USER CODE BEGIN Init */
/* USER CODE END Init */
/* Configure the system clock */
SystemClock_Config();
/* USER CODE BEGIN SysInit */
/* USER CODE END SysInit */
/* Initialize all configured peripherals */
MX_GPIO_Init();
MX_I2C1_Init();
MX_RTC_Init();
/* USER CODE BEGIN 2 */
VL53L0X_DataInit(pMyDevice); //"undefined reference to DataInit"
/* USER CODE END 2 */
/* Infinite loop */
/* USER CODE BEGIN WHILE */
while (1)
{
buff++;
HAL_GPIO_WritePin(GPIOA, GPIO_PIN_1, GPIO_PIN_SET);
HAL_Delay(2000);
HAL_GPIO_WritePin(GPIOA, GPIO_PIN_1, GPIO_PIN_RESET);
HAL_Delay(3000);
/* USER CODE END WHILE */
/* USER CODE BEGIN 3 */
}
/* USER CODE END 3 */
}
2023-04-06 5:22 AM
Hello @ VDein.1
I would start by asking about your project structure :
Waiting your feedback !
Wijeden,
2023-04-06 6:07 AM
1. VL53L0X_DataInit() this function is in the API, exactly in VL53L0X_api.h.
2. Well, I think it is well linked. To use the API import the API library in the Middleswares folder. Then I went to the Project properties and there I added the paths, in C/c++ Build/Settings/MCU GCC Compiler/Include paths.
I don't know if this is the correct way to link the API_VL53L0X files.
Thanks for your time.
VDein.1
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.