STM32CubeIDE (MCUs)

Ask questions on STM32CubeIDE. Discuss how to build, debug, configure, and optimize your project as well as how to use our software tools.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

STM32CubeIDE 2.1.1 released

We are pleased to announce that the minor version 2.1.1 of STM32CubeIDE is available. What is new in 2.1.1: This release covers the topics listed below: SEGGER J-Link GDB server updated to 9.24 to fix an issue with the Live Expression view during the...

Aimen1 by ST Employee
  • 1703 Views
  • 0 replies
  • 1 kudos

STM32CubeCLT 1.21.0 released

We are pleased to announce that STM32CubeCLT 1.21.0 release is available. What is new in 1.21.0: Maintenance of the previous version: Updated in accordance with STM32CubeIDE v2.1.0Update of Clang/LLVM toolchainUpdate of GCC to GCC 14Update of STM32Cu...

Aimen1 by ST Employee
  • 638 Views
  • 0 replies
  • 0 kudos

STM32CubeIDE 2.0 release - early heads-up!

Starting from the release in November 2025, STM32CubeIDE and STM32CubeMX will be available exclusively in their standalone versions. STM32CubeMX will no longer be integrated inside STM32CubeIDE. Instead, the two tools will be interoperable in the sam...

Blinky Program not working for NUCLEO L467RG

I recently purchased a NUCLEO L476RG and originally was able to upload code but now it no longer seems to work.Here is the current firmware version: Pinout is here: Clock configuration: Not quite sure what the issue is here, running the project under...

0693W00000aJiT9QAK.png 0693W00000aJiTEQA0.png 0693W00000aJiTJQA0.png
DRicc.2 by Senior
  • 2811 Views
  • 7 replies
  • 0 kudos

Resolved! I have a debugger issue: When I add a simple variable into the expressions window the value is shown correctly. But for any arrays it reports an error - see details

I use an array, for example, peakindex[6]. The biulder shows no errors. When debugging and looking for the values in the Expressions window the following error messages occur:Multiple errors reported.1) Failed to execute MI command:-var-create - * pe...

USchm.2 by Associate II
  • 5427 Views
  • 3 replies
  • 1 kudos

Resolved! STM32CubeIDE is consuming too much space in C drive

I have been using STM32CubeIDE for the last couple of years. Recently after getting a low space warning in C drive found that  STM32CubeIDE is taking over 32GB of space in C drive. There I found that some libraries are there with previous versions. A...

0693W00000bhD3iQAE.png
MKDas by Associate II
  • 8212 Views
  • 8 replies
  • 0 kudos

Resolved! Hi all.

I have created a project in IAR Embedded Workbench and it is working alright but now due to some reasons I have converted and debugging the same project with same buffer values in STM32cubeide but in this compiler it is showing "region RAM overflowed...

SGoel.2 by Associate III
  • 5827 Views
  • 6 replies
  • 0 kudos
Announcement

We’re moving the ST Community to a new platform to give you a better and more reliable community experience.