2023-08-04 12:20 AM
stmcube ide 1.13.1
.win32_1.1.0.202305231506/tools/bin/../lib/gcc/arm-none-eabi/11.3.1/../../../../arm-none-eabi/bin/ld.exe: C:/ST/STM32CubeIDE_1.13.0/STM32CubeIDE/plugins/com.st.stm32cube.ide.mcu.externaltools.gnu-tools-for-stm32.11.3.rel1.win32_1.1.0.202305231506/tools/bin/../lib/gcc/arm-none-eabi/11.3.1/../../../../arm-none-eabi/lib/thumb/v8-m.main+fp/hard\libc_nano.a(libc_a-gettimeofdayr.o): in function `_gettimeofday_r':
Solved! Go to Solution.
2023-08-04 1:21 AM
@KnarfB wrote:This is a warning, not an error. You can ignore it unless you want to use gettimeofday, in which case you have to implement it yourself for an embedded system :).
hth
KnarfB
I am trying to change the ld file I thought may be because of this my ld file is not refecting
2023-08-04 12:41 AM - edited 2023-08-04 12:42 AM
error message not included?!
2023-08-04 12:44 AM - edited 2023-08-04 12:49 AM
C:/ST/STM32CubeIDE_1.13.0/STM32CubeIDE/plugins/com.st.stm32cube.ide.mcu.externaltools.gnu-tools-for-stm32.11.3.rel1.win32_1.1.0.202305231506/tools/bin/../lib/gcc/arm-none-eabi/11.3.1/../../../../arm-none-eabi/bin/ld.exe: C:/ST/STM32CubeIDE_1.13.0/STM32CubeIDE/plugins/com.st.stm32cube.ide.mcu.externaltools.gnu-tools-for-stm32.11.3.rel1.win32_1.1.0.202305231506/tools/bin/../lib/gcc/arm-none-eabi/11.3.1/../../../../arm-none-eabi/lib/thumb/v8-m.main+fp/hard\libc_nano.a(libc_a-gettimeofdayr.o): in function `_gettimeofday_r':
(.text._gettimeofday_r+0xe): warning: _gettimeofday is not implemented and will always fail
2023-08-04 1:10 AM
This is a warning, not an error. You can ignore it unless you want to use gettimeofday, in which case you have to implement it yourself for an embedded system :).
hth
KnarfB
2023-08-04 1:21 AM
@KnarfB wrote:This is a warning, not an error. You can ignore it unless you want to use gettimeofday, in which case you have to implement it yourself for an embedded system :).
hth
KnarfB
I am trying to change the ld file I thought may be because of this my ld file is not refecting
2023-08-08 5:03 PM
I got the same error after performing "Check for Update" and patching CubeMX to 6.19.1 and CubeIDE to 1.13.1.
This compiling error should be fixed, but no just be ignored.
2023-08-09 11:24 AM
Same here. Tried rebuilding a code from prior CubeMX / CubeIDE version. Prior to the 2 of August 2023.
plugins/com.st.stm32cube.ide.mcu.externaltools.gnu-tools-for-stm32.11.3.rel1.linux64_1.1.0.202305231506/tools/bin/../lib/gcc/arm-none-eabi/11.3.1/../../../../arm-none-eabi/bin/ld:
/home/lawrence/st/stm32cubeide_1.12.1/plugins/com.st.stm32cube.ide.mcu.externaltools.gnu-tools-for-stm32.11.3.rel1.linux64_1.1.0.202305231506/tools/bin/../lib/gcc/arm-none-eabi/11.3.1/../../../../arm-none-eabi/lib/thumb/v7e-m+fp/hard/libc_nano.a(libc_a-gettimeofdayr.o):
in function `_gettimeofday_r': (.text._gettimeofday_r+0xe):
warning: _gettimeofday is not implemented and will always fail
2023-08-10 10:08 AM
I checked the ID file and found no gettimeofday so I don't know where this coming from and how to make it go away or I have to wait for next revision release by ST?
is there code snips to add in gettimeofday
2023-08-11 2:31 AM - edited 2023-08-11 2:32 AM
Guys, I have this problem after IDE upgrade to 1.13.1.
This topic is marked as "solved", but nobody specified how it was solved. Could somebody write the solution, please?
C:/ST/STM32CubeIDE_1.11.2/STM32CubeIDE/plugins/com.st.stm32cube.ide.mcu.externaltools.gnu-tools-for-stm32.11.3.rel1.win32_1.1.0.202305231506/tools/bin/../lib/gcc/arm-none-eabi/11.3.1/../../../../arm-none-eabi/bin/ld.exe: C:/ST/STM32CubeIDE_1.11.2/STM32CubeIDE/plugins/com.st.stm32cube.ide.mcu.externaltools.gnu-tools-for-stm32.11.3.rel1.win32_1.1.0.202305231506/tools/bin/../lib/gcc/arm-none-eabi/11.3.1/../../../../arm-none-eabi/lib/thumb/v7-m/nofp\libc_nano.a(libc_a-gettimeofdayr.o): in function `_gettimeofday_r':
(.text._gettimeofday_r+0xe): warning: _gettimeofday is not implemented and will always fail
2023-08-11 3:24 AM
as KnarfB wrote:
You can ignore it unless you want to use gettimeofday, in which case you have to implement it yourself for an embedded system :).
or if you trust more in compiler :
warning: _gettimeofday is not implemented and will always fail.
solution is : write it yourself.
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.