2023-10-25 1:25 AM - edited 2023-10-25 1:28 AM
I am trying to view and debug the queues in my FreeRTOS project. To do this, I have to add the queues to registry with vQueueAddToRegistry. However, vQueueAddToRegistry takes an argument to a QueueHandle_t and in the project generated with STM32CubeMX I only have queue handles with the type osMessageQueueId_t. How do I get a QueueHandle_t that can be added to registry?
Solved! Go to Solution.
2023-10-25 2:50 AM
Figured this out that I can just do a type cast and it seems the queues are already in the registry as long as the registry size is configured to be big enough in CubeMX.
2023-10-25 2:50 AM
Figured this out that I can just do a type cast and it seems the queues are already in the registry as long as the registry size is configured to be big enough in CubeMX.
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.