2023-02-24 4:00 AM
Hello,
I have a problem with debugger connection.
The first time I had no problems in connecting and debugging my application, but the next times the debugger connects and exit immediately.
I have already tried to close/relaunch STM32CubeIDE, disconnect/reconnect the debug probe, clean any entry in Expressions and Live Expression tabs.
Below I have reported the output console text.
Thank you.
STMicroelectronics ST-LINK GDB server. Version 7.1.0
Copyright (c) 2022, STMicroelectronics. All rights reserved.
Starting server with the following options:
Persistent Mode : Disabled
Logging Level : 1
Listen Port Number : 61234
Status Refresh Delay : 15s
Verbose Mode : Disabled
SWD Debug : Enabled
InitWhile : Enabled
Waiting for debugger connection...
Debugger connected
Waiting for debugger connection...
Debugger connected
Waiting for debugger connection...
-------------------------------------------------------------------
STM32CubeProgrammer v2.12.0
-------------------------------------------------------------------
Log output file: C:\Users\ctaboni\AppData\Local\Temp\STM32CubeProgrammer_a02120.log
ST-LINK SN : 004C001D3331510F34333834
ST-LINK FW : V3J10M3B5S1
Board : STLINK-V3SET
Voltage : 3.28V
SWD freq : 24000 KHz
Connect mode: Under Reset
Reset mode : Hardware reset
Device ID : 0x460
Revision ID : Rev B
Device name : STM32G07x/STM32G08x
Flash size : 128 KBytes
Device type : MCU
Device CPU : Cortex-M0+
BL Version : 0xB2
Debug in Low Power mode enabled
Memory Programming ...
Opening and parsing file: ST-LINK_GDB_server_a02120.srec
File : ST-LINK_GDB_server_a02120.srec
Size : 5.56 KB
Address : 0x08000000
Erasing memory corresponding to segment 0:
Erasing internal memory sectors [0 2]
Download in Progress:
File download complete
Time elapsed during download operation: 00:00:00.190
Verifying ...
Download verified successfully
Shutting down...
Exit.
Solved! Go to Solution.
2023-02-24 5:42 AM
Problem resolved.
I was confused passing from Code Composer to STM32Cube.
I was using a wrong toolbar command that in Code Composer wasn't present.
Thank you,
2023-02-24 5:42 AM
Problem resolved.
I was confused passing from Code Composer to STM32Cube.
I was using a wrong toolbar command that in Code Composer wasn't present.
Thank you,
2024-01-09 6:38 PM
can you tell me resolved way!please
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.