cancel
Showing results for 
Search instead for 
Did you mean: 

CubeIDE: Imported Eclipse 'C' Project incorrectly defines __cplusplus

Andrew Neil
Super User

STM32 CubeIDE v1.5.1; Build: 9029_20201210_1234 (UTC)

The same Eclipse Project as:

https://community.st.com/s/question/0D53W00000Y2lIsSAJ/cant-usecreate-debug-config-for-oss7-stack

It is a 'C' Project, but the CubeIDE defines __cplusplus:

0693W000007ZDYEQA4.png 

Which, as you can see, messes-up the codes checks to see if C++ is being used!

If I manually delete that definition, all is fine.

The problem does not happen when opening the project in a "normal" Eclipse Neon 3.

So why is CubeIDE adding this?

A complex system that works is invariably found to have evolved from a simple system that worked.
A complex system designed from scratch never works and cannot be patched up to make it work.
This discussion is locked. Please start a new topic to ask your question.
33 REPLIES 33

When you "delete" from within the IDE, that just takes things out of the workspace - there is an option to also delete them from the filesystem ...

A complex system that works is invariably found to have evolved from a simple system that worked.
A complex system designed from scratch never works and cannot be patched up to make it work.

Wow - that is a radical move... :)

I don't even have a theory as to why this did not work in the first place for you.

Can you re-produce it in some way again? Maybe you could export an old tag of the project, where it is not working, assuming the project is under version control? If so, I can try it on my side...

Hi Mattias, I'm running into the issue again. I have attached 4 versions of the .cproject file, saved in various states of trying to get the MCU choice box to become enabled. I am using IDE v1.8.0.

Any help is appreciated!

I ran into this problem again today, and this time it didn't matter how many times I removed and re-created the project in the project tree, the MCU selection was always greyed out. The only thing that fixed the issue was to delete all .*project files.

Further, when I was finally able to select an MCU using the workaround method, the options for FPU were all set to "software". Odd given this part has a hardware FPU.

Announcement

We’re moving the ST Community to a new platform to give you a better and more reliable community experience.