cancel
Showing results for 
Search instead for 
Did you mean: 

Cube IDE 1.15.0

Parmin Nayani
Associate III

Hi all,

Installed the latest CubeIDE and re-built an existing project. Got several warnings. One of them was 

RWX. This could be solved by making changes to the ,ld file. Example - .ARM (READONLY)

The next issues was -- > "_close is not implemented and will always fail". Don't know how to solve this warning.

I believe these problems are due to latest version GCC.

Another issue I noticed is - memory regions have disappeared. I have a correctly name list file but to no avail.

Can someone please help me solve these issues. Please help. Thanks.

 

NPS 

 

This discussion is locked. Please start a new topic to ask your question.
12 REPLIES 12

Here is the project

Hello @Parmin Nayani 

This is a known issue that will be fixed on the next releases. As a temporary workaround, in main.c file, add these instructions: 

__attribute__((weak)) void _close(void){} 
__attribute__((weak)) void _lseek(void){} 
__attribute__((weak)) void _read(void){} 
__attribute__((weak)) void _write(void){}

Between "/* USER CODE BEGIN Includes */" and "/* USER CODE END Includes */".

Best Regards.

STTwo-32

 

To give better visibility on the answered topics, please click on Accept as Solution on the reply which solved your issue or answered your question.

Hi STTwo-32,

Thank you for the update.  Now I am not getting the warning. Hopefully nothing else is getting disturbed. Thank you.

 

Announcement

We’re moving the ST Community to a new platform to give you a better and more reliable community experience.