2024-03-29 2:08 PM
I am currently trying to test my PCB that I made using the STM32F407VGT6 microcontroller. I have my code to toggle a led using a gpio output pin on the controller connected to the led on a breadboard. Under the system core on STM32IDE I have the SYS configuration set to serial wire for the debug mode and the timebase source to SysTick. When I go to run my code which is just the simple code to toggle the led on and off, I get this message: "unexpected flash size for ST-Link micro. Don't know how to upgrade."
I'm not sure how to go about debugging the problem as I have done some digging to try and find out what the solution to this could be.
2024-04-01 6:57 AM - edited 2024-04-01 6:58 AM
Hello @keatonr,
Are you using STLinkUpgrade version 3.14.5?
I think you have the same issue reported in this post. This is an issue with STLinkUpgrade.jar v3.14.5 and this will be fixed in the coming release of STLinkUpgrade.
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.