cancel
Showing results for 
Search instead for 
Did you mean: 

Cube IDE 1.15.0

Parmin Nayani
Associate III

Hi all,

Installed the latest CubeIDE and re-built an existing project. Got several warnings. One of them was 

RWX. This could be solved by making changes to the ,ld file. Example - .ARM (READONLY)

The next issues was -- > "_close is not implemented and will always fail". Don't know how to solve this warning.

I believe these problems are due to latest version GCC.

Another issue I noticed is - memory regions have disappeared. I have a correctly name list file but to no avail.

Can someone please help me solve these issues. Please help. Thanks.

 

NPS 

 

This discussion is locked. Please start a new topic to ask your question.
1 ACCEPTED SOLUTION

Accepted Solutions

Hello @Parmin Nayani 

This is a known issue that will be fixed on the next releases. As a temporary workaround, in main.c file, add these instructions: 

__attribute__((weak)) void _close(void){} 
__attribute__((weak)) void _lseek(void){} 
__attribute__((weak)) void _read(void){} 
__attribute__((weak)) void _write(void){}

Between "/* USER CODE BEGIN Includes */" and "/* USER CODE END Includes */".

Best Regards.

STTwo-32

 

To give better visibility on the answered topics, please click on Accept as Solution on the reply which solved your issue or answered your question.

View solution in original post

12 REPLIES 12
STTwo-32
ST Employee

Hello @Parmin Nayani 

Could you please take a look at this post. It should be helpful.

Best Regards.

STTwo-32

To give better visibility on the answered topics, please click on Accept as Solution on the reply which solved your issue or answered your question.

Hi,

I seem to miss "Could you please take a look at this post. It should be helpful." link. Can you post the link please? Thank you.

Hello @Parmin Nayani 

I've added the link sorry for this mistake.

Best Regards.

STTwo-32

To give better visibility on the answered topics, please click on Accept as Solution on the reply which solved your issue or answered your question.

Hi STTwo-32,

I did as suggested but the warnings are persisting.  Here are the warnings

C:/ST/STM32CubeIDE_1.15.0/STM32CubeIDE/plugins/com.st.stm32cube.ide.mcu.externaltools.gnu-tools-for-stm32.12.3.rel1.win32_1.0.100.202403111256/tools/bin/../lib/gcc/arm-none-eabi/12.3.1/../../../../arm-none-eabi/bin/ld.exe: C:/ST/STM32CubeIDE_1.15.0/STM32CubeIDE/plugins/com.st.stm32cube.ide.mcu.externaltools.gnu-tools-for-stm32.12.3.rel1.win32_1.0.100.202403111256/tools/bin/../lib/gcc/arm-none-eabi/12.3.1/../../../../arm-none-eabi/lib/thumb/v7-m/nofp\libc_nano.a(libc_a-closer.o): in function `_close_r':

(.text._close_r+0xc): warning: _close is not implemented and will always fail

C:/ST/STM32CubeIDE_1.15.0/STM32CubeIDE/plugins/com.st.stm32cube.ide.mcu.externaltools.gnu-tools-for-stm32.12.3.rel1.win32_1.0.100.202403111256/tools/bin/../lib/gcc/arm-none-eabi/12.3.1/../../../../arm-none-eabi/bin/ld.exe: C:/ST/STM32CubeIDE_1.15.0/STM32CubeIDE/plugins/com.st.stm32cube.ide.mcu.externaltools.gnu-tools-for-stm32.12.3.rel1.win32_1.0.100.202403111256/tools/bin/../lib/gcc/arm-none-eabi/12.3.1/../../../../arm-none-eabi/lib/thumb/v7-m/nofp\libc_nano.a(libc_a-lseekr.o): in function `_lseek_r':

(.text._lseek_r+0x10): warning: _lseek is not implemented and will always fail

C:/ST/STM32CubeIDE_1.15.0/STM32CubeIDE/plugins/com.st.stm32cube.ide.mcu.externaltools.gnu-tools-for-stm32.12.3.rel1.win32_1.0.100.202403111256/tools/bin/../lib/gcc/arm-none-eabi/12.3.1/../../../../arm-none-eabi/bin/ld.exe: C:/ST/STM32CubeIDE_1.15.0/STM32CubeIDE/plugins/com.st.stm32cube.ide.mcu.externaltools.gnu-tools-for-stm32.12.3.rel1.win32_1.0.100.202403111256/tools/bin/../lib/gcc/arm-none-eabi/12.3.1/../../../../arm-none-eabi/lib/thumb/v7-m/nofp\libc_nano.a(libc_a-readr.o): in function `_read_r':

(.text._read_r+0x10): warning: _read is not implemented and will always fail

C:/ST/STM32CubeIDE_1.15.0/STM32CubeIDE/plugins/com.st.stm32cube.ide.mcu.externaltools.gnu-tools-for-stm32.12.3.rel1.win32_1.0.100.202403111256/tools/bin/../lib/gcc/arm-none-eabi/12.3.1/../../../../arm-none-eabi/bin/ld.exe: C:/ST/STM32CubeIDE_1.15.0/STM32CubeIDE/plugins/com.st.stm32cube.ide.mcu.externaltools.gnu-tools-for-stm32.12.3.rel1.win32_1.0.100.202403111256/tools/bin/../lib/gcc/arm-none-eabi/12.3.1/../../../../arm-none-eabi/lib/thumb/v7-m/nofp\libc_nano.a(libc_a-writer.o): in function `_write_r':

(.text._write_r+0x10): warning: _write is not implemented and will always fail

C:/ST/STM32CubeIDE_1.15.0/STM32CubeIDE/plugins/com.st.stm32cube.ide.mcu.externaltools.gnu-tools-for-stm32.12.3.rel1.win32_1.0.100.202403111256/tools/bin/../lib/gcc/arm-none-eabi/12.3.1/../../../../arm-none-eabi/bin/ld.exe: warning: 12CSN_card_reader.elf has a LOAD segment with RWX permissions

Finished building target: 12CSN_card_reader.elf

No problems. The problem still persists. Please help. Thank you.

Could you upload your project here.

Best Regards.

STTwo-32

To give better visibility on the answered topics, please click on Accept as Solution on the reply which solved your issue or answered your question.

Can you please elaborate on the project file? What files do you want me to send? 

The warning is for stm32f103c8 controller. I have project for 407 but that compiles without warnings.

Send all the Project on one of the supported formats on this community (.7z for example).

Best Regards.

STTwo-32

To give better visibility on the answered topics, please click on Accept as Solution on the reply which solved your issue or answered your question.

Announcement

We’re moving the ST Community to a new platform to give you a better and more reliable community experience.