STM32CubeIDE (MCUs)

Ask questions on STM32CubeIDE. Discuss how to build, debug, configure, and optimize your project as well as how to use our software tools.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

STM32CubeIDE 2.1.1 released

We are pleased to announce that the minor version 2.1.1 of STM32CubeIDE is available. What is new in 2.1.1: This release covers the topics listed below: SEGGER J-Link GDB server updated to 9.24 to fix an issue with the Live Expression view during the...

Aimen1 by ST Employee
  • 1703 Views
  • 0 replies
  • 1 kudos

STM32CubeCLT 1.21.0 released

We are pleased to announce that STM32CubeCLT 1.21.0 release is available. What is new in 1.21.0: Maintenance of the previous version: Updated in accordance with STM32CubeIDE v2.1.0Update of Clang/LLVM toolchainUpdate of GCC to GCC 14Update of STM32Cu...

Aimen1 by ST Employee
  • 638 Views
  • 0 replies
  • 0 kudos

STM32CubeIDE 2.0 release - early heads-up!

Starting from the release in November 2025, STM32CubeIDE and STM32CubeMX will be available exclusively in their standalone versions. STM32CubeMX will no longer be integrated inside STM32CubeIDE. Instead, the two tools will be interoperable in the sam...

How to program stm32h757xi microcontroller

I want to explore dual core processor so i was going through stm32h757xi microcontroller which has dual core microcontroller. As currently i was working on stm32g4 microntroller for which i have made custom pcb in that for programming i have used ser...

Shubham08 by Associate III
  • 892 Views
  • 1 replies
  • 1 kudos

Resolved! Debug a basic C++ program on STMCube IDE

Here's my infinite loop in a cpp file  #include "main.h" #include "lib.hpp" void run() { auto cnt = 0u; while (1) { if(!HAL_GPIO_ReadPin(GPIOC, GPIO_PIN_13)) cnt++; } }I run the Debugger and execute the statements until I get to the "if" ...

TechyAry by Associate III
  • 3743 Views
  • 13 replies
  • 7 kudos

Resolved! STM32CubeIDE crashes on opening 'Software Packs'

Hello AllI'm using STM32CubeIDE 1.18.1 on a Windows 11 (10.0.26100) virtual machine through VirtualBox (7.1.8).I've been able to create a project for my board and generate code, however when I go to the software packs, it causes the IDE to consistent...

dbit_0-1748265620780.png
dbit by Associate II
  • 1823 Views
  • 3 replies
  • 1 kudos

Cannot Download STM32CUBEIDE Software

I am unable to download any of the STM32CUBEIDE software from https://www.st.com/en/development-tools/stm32cubeide.html#. Everytime I log in and press download, the download bar always stays at 0% no matter what. This does not occur with any other do...

Haoming_Mei_0-1748814470483.png

Resolved! Nucleo-Board Not Supported By CUBE-IDE

Hello every ones, I am tring to start a new project by exploring some new nucleo board that i see on stmicroelectronics web site. If I select the NUCLEO-H7S3L8 board i can't start the creation of the project because CUBE IDE say that: "The target dev...

SMusc.1 by Senior
  • 1046 Views
  • 1 replies
  • 0 kudos

Resolved! Enabling printf on NUCLEO-N657 in STM32CubeIDE

I have enabled Serial Wire Viewer (SWV) in my m55 application as I have done with my m4 and m33 projects, but the printf is not appearing in the SWV view.Are there additional setup required on the NUCLEO-N657 board such as jumper settings or addition...

Resolved! MCU packages "from Local"

Hello,My network is blocked, so can't access the packages through CubeIDE.I am trying to add the MCU package "from Local" as mentioned in the thread https://community.st.com/t5/stm32cubeide-mcus/unbale-to-connect-to-the-network/m-p/118945/highlight/t...

gits007_0-1748606452561.png gits007_1-1748606760097.png
gits007 by Associate
  • 1080 Views
  • 1 replies
  • 1 kudos
Announcement

We’re moving the ST Community to a new platform to give you a better and more reliable community experience.