2025-05-26 6:27 AM
Hello All
I'm using STM32CubeIDE 1.18.1 on a Windows 11 (10.0.26100) virtual machine through VirtualBox (7.1.8).
I've been able to create a project for my board and generate code, however when I go to the software packs, it causes the IDE to consistently crash.
I have so far attempted to no success:
My .metadata/.log is as follows - repeated many times:
(I have also attempted to install STM32CubeMX but have been unsuccessful, probably unrelated)
Does anyone have any ideas or solutions? - A quick scan of the forum didn't come up with anything
My local installation of the IDE works (and gives the same .log errors) however that isn't a viable solution for me in the long term.
Thanks in advance.
Solved! Go to Solution.
2025-06-02 1:48 AM
Given that the software simply does not work with the Windows 11 environment stated above. For anyone following along I have resolved my issue by the following:
Changed the VM to Windows 10 (Windows 10 Pro, 19045.4529). Using the software:
2025-05-27 1:05 AM
Hello @dbit
First let me thank you for posting.
Let's try the following steps :
1- Check Virtual Machine configuration: Ensure that your virtual machine has sufficient resources allocated (CPU, RAM) to run STM32CubeIDE smoothly.
2- Verify that the virtual machine's network settings allow it to access the internet, as this might be necessary for downloading software packs.
3- Try to follow the steps mentioned in this Article How to set the network connection parameters for STM32CubeIDE and STM32CubeMX
4- Try creating a new workspace : New-->Switch workspace-->other-->Create a new workspace
If the problem persist , manually download the software packs from the STMicroelectronics website and install them offline. This can sometimes bypass issues related to network or IDE settings.
I will be waiting for your feedback.
THX
Ghofrane
To give better visibility on the answered topics, please click on Accept as Solution on the reply which solved your issue or answered your question.
2025-05-27 2:01 AM
Thanks for getting back to me.
I have downloaded a package to try and load it 'offline' using the {Help -> Configuration Tool -> Manage Embedded Software Packages} and adding from local. Fortunately I can also download packs from this menu, which is a step forward, thank you.
Unfortunately my issue is not resolved as when I attempt to use or configure the package the 'Software Packs Component Selector' screen is brought up, thus crashing the program.
Do you know why this would be happening?
Thanks.
2025-06-02 1:48 AM
Given that the software simply does not work with the Windows 11 environment stated above. For anyone following along I have resolved my issue by the following:
Changed the VM to Windows 10 (Windows 10 Pro, 19045.4529). Using the software:
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.