STM32CubeIDE (MCUs)

Ask questions on STM32CubeIDE. Discuss how to build, debug, configure, and optimize your project as well as how to use our software tools.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

STM32CubeIDE 2.1.1 released

We are pleased to announce that the minor version 2.1.1 of STM32CubeIDE is available. What is new in 2.1.1: This release covers the topics listed below: SEGGER J-Link GDB server updated to 9.24 to fix an issue with the Live Expression view during the...

Aimen1 by ST Employee
  • 1703 Views
  • 0 replies
  • 1 kudos

STM32CubeCLT 1.21.0 released

We are pleased to announce that STM32CubeCLT 1.21.0 release is available. What is new in 1.21.0: Maintenance of the previous version: Updated in accordance with STM32CubeIDE v2.1.0Update of Clang/LLVM toolchainUpdate of GCC to GCC 14Update of STM32Cu...

Aimen1 by ST Employee
  • 638 Views
  • 0 replies
  • 0 kudos

STM32CubeIDE 2.0 release - early heads-up!

Starting from the release in November 2025, STM32CubeIDE and STM32CubeMX will be available exclusively in their standalone versions. STM32CubeMX will no longer be integrated inside STM32CubeIDE. Instead, the two tools will be interoperable in the sam...

Resolved! How to change the STM32 family in a project using HAL?

Hello,I am currently using a F4 processor in HAL together with the Stm32cubeIDE.Thus the IDE generates F4 hal files which later are included in the main program.  To access the specific functions I need to #include "stm32f4xx_hal.h" in my own program...

DocAlex by Associate III
  • 1750 Views
  • 5 replies
  • 2 kudos

Cube IDE freezed after draining free physical memory

It does it only on one PC out of several, however.More details here (EEVBLOG link, not dodgy, had to do this because this forum cuts pieces out of URLs to other forums)https://tinyurl.com/4r5uwt2s I've tried the Xmx1024m stmcubeide.ini file parameter...

PHolt.1 by Senior III
  • 821 Views
  • 2 replies
  • 1 kudos

STM32CubeIDE 1.18.1 released

We are pleased to announce that the minor release 1.18.1 of STM32CubeIDE is available. What is new in 1.18.1: This minor release will not bring any major updates to the STM32CubeIDE 1.18.1. It will be aligned with the STM32CubeMX 6.14.1. Main fixed i...

STLINK in Nucleo-H753ZI board stopped working

Hi,     My STLINK for debug in Nucleo-H753ZI board stopped working.      It was working when entering the debug mode.      Now, it stopped working.- I got the error message -  1. "Error in initializing ST link device." 2. "Failed to execute M1 comman...

Resolved! No code generated for inline function call

There is no code generated for the led_rgb_toggle() call here:led_rgb_toggle() is an inline function:static inline void led_rgb_toggle( GPIO_PinState r_state, GPIO_PinState g_state, GPIO_PinState b_state ) { #if defined PROJECT_WITH_RGB_LEDS if( ...

AndrewNeil_0-1751021380876.png AndrewNeil_2-1751022078656.png
Announcement

We’re moving the ST Community to a new platform to give you a better and more reliable community experience.