STM32CubeIDE (MCUs)

Ask questions on STM32CubeIDE. Discuss how to build, debug, configure, and optimize your project as well as how to use our software tools.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

STM32CubeIDE 2.1.1 released

We are pleased to announce that the minor version 2.1.1 of STM32CubeIDE is available. What is new in 2.1.1: This release covers the topics listed below: SEGGER J-Link GDB server updated to 9.24 to fix an issue with the Live Expression view during the...

Aimen1 by ST Employee
  • 1703 Views
  • 0 replies
  • 1 kudos

STM32CubeCLT 1.21.0 released

We are pleased to announce that STM32CubeCLT 1.21.0 release is available. What is new in 1.21.0: Maintenance of the previous version: Updated in accordance with STM32CubeIDE v2.1.0Update of Clang/LLVM toolchainUpdate of GCC to GCC 14Update of STM32Cu...

Aimen1 by ST Employee
  • 638 Views
  • 0 replies
  • 0 kudos

STM32CubeIDE 2.0 release - early heads-up!

Starting from the release in November 2025, STM32CubeIDE and STM32CubeMX will be available exclusively in their standalone versions. STM32CubeMX will no longer be integrated inside STM32CubeIDE. Instead, the two tools will be interoperable in the sam...

Resolved! CubeIDE device configuration no longer opens.

Good day, everyone. I've got an issue where after creating the project with the startup CubeIDE, (which I presume is also CubeMX just running from within the IDE) It seems that I can no longer launch the MX window in order to change or add some thing...

0690X00000ArblUQAR.png
MThat by Associate II
  • 1513 Views
  • 1 replies
  • 1 kudos

Modifying tick period to 0.01 millisecond has no effect in generated code (default is 1 millisec or 1 KHz frequency) with TIM8 as Timebase source in System configuration.

Hi,Am using STM32CubeIDE with FreeRTOS middleware (CMSISv1). I dont see change in code generated in file stm32f4xx_hal_timebase_tim.c when I modify tick frequency to 100000 instead of the default 1000. In sys tab of configuration setting TIM8 as time...

DevBee by Associate II
  • 1648 Views
  • 1 replies
  • 0 kudos

Automatic choice of a header by a used STM.

Hi! I have the own include file which contains more the same HAL libraries headers with a different types of controllers. Could it be some possible (with Directive and Contitions?) for a compiler to choose itself according to the used controller in...

Filipx.87 by Associate II
  • 1351 Views
  • 2 replies
  • 0 kudos

How import mbed project on stm32 cubeide?

Hello everyone, this is my firt question, sorry for my error. I have create a little program on mbed online compiler, but now i would import this program on stm32cubeide for use debug. Online i have see some tutorial but they are old and don't work. ...

Why don't user debug scripts work with STM32CubeIDE ?

When I specify a user debug script in STM32CubeIDE debug configuration window I get the error "Provided file doesn't exist" even though it's there. Even if I specify the same text as the "Automated Generation" option I get this error.Is there a worka...

0690X000009YeY2QAK.jpg
dave2012 by Associate III
  • 2922 Views
  • 10 replies
  • 0 kudos
Announcement

We’re moving the ST Community to a new platform to give you a better and more reliable community experience.