2019-10-31 11:04 AM
Hi! I have the own include file which contains more the same HAL libraries headers with a different types of controllers. Could it be some possible (with Directive and Contitions?) for a compiler to choose itself according to the used controller in Project? Thanx.
I always have to choose manually...
// #include "stm32l1xx_hal.h"
#include "stm32f1xx_hal.h"
//#include "stm32f4xx_hal.h"
// #include "stm32f7xx_hal.h"
2019-10-31 11:29 AM
Doesn't the compiler command line, by way of the project meta-data, get a definition passed of the platform/cpu being used?
ie STM32L432xx
And things like
#if defined (STM32L412xx) || defined (STM32L422xx) || defined (STM32L431xx) || defined (STM32L432xx) || defined (STM32L433xx) || defined (STM32L442xx) || defined (STM32L443xx) || defined (STM32L451xx) || defined (STM32L452xx) || defined (STM32L462xx) || defined (STM32L4R5xx) || defined (STM32L4R7xx) || defined (STM32L4R9xx) || defined (STM32L4S5xx) || defined (STM32L4S7xx) || defined (STM32L4S9xx)
/* The temperature sensor measurement path (channel 17) is available on ADC1 */
#define ADC_TEMPERATURE_SENSOR_INSTANCE(__HANDLE__) (((__HANDLE__)->Instance) == ADC1)
#elif defined (STM32L471xx) || defined (STM32L475xx) || defined (STM32L476xx) || defined (STM32L485xx) || defined (STM32L486xx) || defined (STM32L496xx) || defined (STM32L4A6xx)
/* The temperature sensor measurement path (channel 17) is available on ADC1 and ADC3 */
#define ADC_TEMPERATURE_SENSOR_INSTANCE(__HANDLE__) ((((__HANDLE__)->Instance) == ADC1) || (((__HANDLE__)->Instance) == ADC3))
#endif
OR
#if defined(STM32L1) || defined(STM32L4) || defined(STM32G0) || defined(STM32L5)
#define HAL_DAC_MSP_INIT_CB_ID HAL_DAC_MSPINIT_CB_ID
#define HAL_DAC_MSP_DEINIT_CB_ID HAL_DAC_MSPDEINIT_CB_ID
#endif
2019-10-31 11:36 AM
STM32 headers are meant to be used like this:
#define STM32F767xx
#define USE_HAL_DRIVER
#include "stm32f7xx.h"Or you can put those defines in a project configuration.
But, if you're building a single project for multiple boards, you should have some BSP layer. Then you can put MCU specific defines and includes in BSP files.
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.