2019-11-01 9:56 PM
Good day, everyone. I've got an issue where after creating the project with the startup CubeIDE, (which I presume is also CubeMX just running from within the IDE) It seems that I can no longer launch the MX window in order to change or add some things. Anyone has an idea why this is the case?
Neither these, nor the MX button at the top right end of the window do anything.
Solved! Go to Solution.
2019-11-02 2:19 PM
Ah, I figured it out. I have to double click on the .ioc file to open the built in cubeMX tool again.
2019-11-02 2:19 PM
Ah, I figured it out. I have to double click on the .ioc file to open the built in cubeMX tool again.
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.