STM32CubeIDE (MCUs)

Ask questions on STM32CubeIDE. Discuss how to build, debug, configure, and optimize your project as well as how to use our software tools.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

STM32CubeIDE 2.1.1 released

We are pleased to announce that the minor version 2.1.1 of STM32CubeIDE is available. What is new in 2.1.1: This release covers the topics listed below: SEGGER J-Link GDB server updated to 9.24 to fix an issue with the Live Expression view during the...

Aimen1 by ST Employee
  • 1703 Views
  • 0 replies
  • 1 kudos

STM32CubeCLT 1.21.0 released

We are pleased to announce that STM32CubeCLT 1.21.0 release is available. What is new in 1.21.0: Maintenance of the previous version: Updated in accordance with STM32CubeIDE v2.1.0Update of Clang/LLVM toolchainUpdate of GCC to GCC 14Update of STM32Cu...

Aimen1 by ST Employee
  • 638 Views
  • 0 replies
  • 0 kudos

STM32CubeIDE 2.0 release - early heads-up!

Starting from the release in November 2025, STM32CubeIDE and STM32CubeMX will be available exclusively in their standalone versions. STM32CubeMX will no longer be integrated inside STM32CubeIDE. Instead, the two tools will be interoperable in the sam...

HAL libraries and LL libraries version & download links.

Hello,I am comparing the STM32Cube IDE (the suggested from ST) and OpenSTM32 IDE HAL system organization and I have a few questions about it:Is there a way to know the HAL libraries version ? Actually I don't see this parameter.Is it possible to down...

simo zz by Senior II
  • 2986 Views
  • 1 replies
  • 1 kudos

Resolved! Create an assembly project

Hi, For education purpose, I'm trying to create, compile, load and debug assembly projects with STM32Cube. Unfortunately, there are no built in options to do it. I noticed that I can erase on an existing project the main.c and create a main.s instead...

SToru.1 by Associate
  • 4356 Views
  • 2 replies
  • 0 kudos

STM32Cube 1.3.0 - Error: bind failed. Error = 98, exit

Hi,I am using STM32CubeIDE 1.3.0 on Linux Debian, and when I try to flash the MCU using the Run Button, GDB fails with error "bind failed. Error = 98, exit" (it seems that the IDE is trying to open an busy connection).Concretely the log from console ...

simo zz by Senior II
  • 1405 Views
  • 1 replies
  • 1 kudos

bug report: STM32F302CBT6 failed to compile

Hi, This particular MCU is not fully populate in project generator, the result when trying to create a project is incomplete project that can't compile. I worked-around by selecting a different MCU, but as migrating between MCU is not supported, I am...

BVauc.1 by Associate II
  • 1661 Views
  • 3 replies
  • 0 kudos

Having trouble understanding how to copy a project.

For Reference I have used IAR for 10+ years, now migrating to STM32CubeIDE for all future development. For clarity, my issue described below has nothing to do with transitioning from 1 platform to another.My issue is if I copy project A to project B,...

Valid RAM area shows as "????????" in Memory window

Hi,I'm debugging a STM32F765 application using STM32CubeIDE v1.3.1 with ST-Link/V3 debug adapter via OpenOCD.The Memory window shows a gap of 800 RAM bytes in a valid RAM area (see picture below). Any idea what can cause this ?ThanksDave

0693W000000Wo5FQAS.jpg
dave2012 by Associate III
  • 2792 Views
  • 5 replies
  • 0 kudos

Semihosting on the STM32CubeIDE version 1.3

Hi All,I running STM32CubeIDE on Ubuntu mate 20.04 and was wondering if there has been any progress in the area of using Semihosting working on STM32CubeIDE version 1.3 without OpenOCD.I am developing on STM32L073 and would like to get this feature w...

onio by Senior
  • 826 Views
  • 0 replies
  • 0 kudos
Announcement

We’re moving the ST Community to a new platform to give you a better and more reliable community experience.